Failed to download a project on a MIMXRT1160-EVK board.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Failed to download a project on a MIMXRT1160-EVK board.

Jump to solution
1,714 Views
john71
Senior Contributor I

The board (MIMXRT1166_EVK) is powered up and connected with a provided USB cable to J11.

When I run Debug I get

 

MCUXpresso IDE RedlinkMulti Driver v11.4 (Sep 13 2021 15:04:52 - crt_emu_cm_redlink build 16)
Found chip XML file in D:/Workspace_MCUXpresso_11.4/MIMXRT1166_EVK_CM4/Debug\MIMXRT1166xxxxx.xml
Reconnected to existing LinkServer process.
not running connect script in attach mode
Probe Firmware: DAPLink CMSIS-DAP (ARM)
Serial Number:  024400000208827100000000000000000000000097969905
VID:PID:  0D28:0204
USB Path: \\?\hid#vid_0d28&pid_0204&mi_03#9&350958c4&0&0000#{4d1e55b2-f16f-11cf-88cb-001111000030}
Using memory from core 1 after searching for a good core
Using memory from core 1 after searching for a good core
Using memory from core 1 after searching for a good core
connection failed - Nn(05). Wire ACK Wait in DAP access.. Retrying
Using memory from core 1 after searching for a good core
Using memory from core 1 after searching for a good core
Using memory from core 1 after searching for a good core
Failed on connect: Nn(05). Wire ACK Wait in DAP access
Connected&Reset. Was: NotConnected. DpID: 6BA02477. CpuID: 00000000. Info: <None>
Last stub error 0: OK
Last sticky error: 0x0 AIndex: 1
Debug bus selected: MemAp 1
DAP Speed test unexecuted or failed
Debug protocol: SWD. RTCK: Disabled. Vector catch: Disabled.
(100) Target Connection Failed
error closing down debug session - Nn(05). Wire ACK Wait in DAP access

 

What should I set in MCUXpresso IDE or on the board to get it working?

0 Kudos
Reply
1 Solution
1,693 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @john71 ,

   Please don't worry.

   As I know, the MCUXpresso IDE can debug the CM4 core, but you need to download the CM7 at first, that's why I recommend you download the CM7 project, please refer to this post about 2 core debug in mcuxpresso:

https://community.nxp.com/t5/i-MX-RT-Knowledge-Base/How-to-use-JLINK-to-debug-RT1170-dual-core/ta-p/...

Best Regards,

Kerry

View solution in original post

4 Replies
1,703 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @john71 ,

  Please download the SDK at first for the RT1160-EVK:

https://mcuxpresso.nxp.com/en/builder?hw=MIMXRT1160-EVK

Then refer to the Getting Started with MCUXpresso SDK for MIMXRT1160-EVK.pdf in folder:

SDK_2_10_0_MIMXRT1160-EVK\docs

kerryzhou_0-1634706055366.png

You need to download the CM7 project instead of the CM4, and SW1[1:4] should be 0010.

 

Please try it again.

Wish it helps you!

If you still have questions about it, please kindly let me know.

Best Regards,

Kerry

 

0 Kudos
Reply
1,698 Views
john71
Senior Contributor I

Hi Kerry,

Thank you for the answer. Frankly - I'm shocked. I need two cores - that's the reason  I choose the chip.

What chip do allow us to debug both cores? At design time I can drift to other chip.

 

 

0 Kudos
Reply
1,694 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @john71 ,

   Please don't worry.

   As I know, the MCUXpresso IDE can debug the CM4 core, but you need to download the CM7 at first, that's why I recommend you download the CM7 project, please refer to this post about 2 core debug in mcuxpresso:

https://community.nxp.com/t5/i-MX-RT-Knowledge-Base/How-to-use-JLINK-to-debug-RT1170-dual-core/ta-p/...

Best Regards,

Kerry

1,686 Views
john71
Senior Contributor I

Thank you. This way it works. If I run CM7 first I can debug CM4 then.

0 Kudos
Reply