How do I choose a double precision hardware FPU in the MCUXpresso project settings?
The FPU type selectors are confusing and does not seem to match with ARM documentation.
I need hardware double-precision floating point.
On Arm's documentation, the option for double precision is given as FPv5-DP-D16-M, and the MCUXpresso does not let me choose that.
Thanks
Perhaps also check the actual compiler command line being used, I think you need both -mfpu=fpv5-d16 and -mfloat-abi=hard.
-Nick
Hi
is correct for i.MX RT parts with double-precision FPU.
For those with only single-precision (i.MX RT 1011) the FPv5-SP16(Hard ABI) can be used instead.
Regards
Mark
[uTasker project developer for Kinetis and i.MX RT]
Contact me by personal message or on the uTasker web site to discuss professional training, solutions to problems or rapid product development requirements
For professionals searching for faster, problem-free Kinetis and i.MX RT 10xx developments the uTasker project holds the key: https://www.utasker.com/iMX/RT1064.html