FOTA using ethernet or MQTT in IMXRT1064

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FOTA using ethernet or MQTT in IMXRT1064

900 Views
karthik1
Contributor I

1.Any API to do operation on internal flash  in IMXRT1064?

1.Please suggest me the approach to do FOTA update using Ethernet (application program to download the firmware  into external flash hyperflash/ QSPI NOR flash )  in imxRT1064 board.?

2.Amazon FreeRTOS  OTA demo code is supported for imxRT1060 but not given SDK Amazon FreeRTOS  OTA demo code for imxRT1064 ,is it available for IMXRT1064 board?

3. Any suggestion using secondary bootloader to do FOTA?

 

0 Kudos
1 Reply

795 Views
FelipeGarcia
NXP Employee
NXP Employee

This is a duplicated thread. Please refer to this post: https://community.nxp.com/thread/522713 

0 Kudos