FLEX SPI frequency set

cancel
Showing results for 
Search instead for 
Did you mean: 

FLEX SPI frequency set

195 Views
adi2Intel
Contributor II

Hello,

we’re testing flexspi in the following configuration:

 

static inline void FLEXSPI_ClockInit(void)

{

    const clock_usb_pll_config_t g_ccmConfigUsbPll = {.loopDivider = 0U};

 

    CLOCK_InitUsb1Pll(&g_ccmConfigUsbPll);

    CLOCK_InitUsb1Pfd(kCLOCK_Pfd0, 24);   /* Set PLL3 PFD0 clock 360MHZ. */

    CLOCK_SetMux(kCLOCK_FlexspiMux, 0x0); /* Choose PLL3 PFD0 clock as flexspi source clock. */

    CLOCK_SetDiv(kCLOCK_FlexspiDiv, divider);

}

 

and measuring frequency. For divider 2 the frequency is ~25MHz, and for divider 7 the frequency ~9MHz.

We’re interesting to reduce the frequency to ~3MHz, is there is any way to do it?

 

Thanks!


Adi,

Intel

Tags (3)
0 Kudos
1 Reply

186 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @adi2Intel ,

    About the flexspi clock setting, you totally can use the MCUXPresso IDE CFG clock to configure it:

kerryzhou_0-1648784813147.png

The divide max is 8, if after 8 divider, still can't match your required frequency.

Then you need to cut down the flexSPI source code, just use the CFG tool to configure it, more easy.

 

Best Regards,

Kerry

 

0 Kudos