F_mount returning FR_NOT_READY

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

F_mount returning FR_NOT_READY

1,376 Views
Alberto_isorna
Contributor II

I'm trying to implement a card writting in the csi_RGB565 example.

 

When I try to read a file and I mount the disk I have the following error:

FR_NOT_READY

Could you please help me to solve the issue?

(When I perform the sd_jpeg example with the SAME card it works well, I don"t understand, I already routed the same ports and periphericals, please help)

Find the main attached, if you need more info please ask me. 

Labels (1)
0 Kudos
2 Replies

1,344 Views
Alberto_isorna
Contributor II

Hello, 

Thanks for your answer, indeed the problem was that in ffconf.h it was : #define RAM_DISK_ENABLE instead of SD_DISK_ENABLE

After that everything was OK.

Best regards,

Alberto.

0 Kudos

1,360 Views
FelipeGarcia
NXP Employee
NXP Employee

Hi Alberto,

Could you please provide the steps you have done on your side so I can replicate this same issue with my board? Also please check pins and clocks initialization is the same as in the sd_jpeg example.

Best regards,

Felipe

0 Kudos