Hi,
Is there some example of external watchdog implementation in i.MXRT1024 & what should I do to implement it?
Hi @sowmiya_a,
You can find examples of the External Watchdog Monitor (EWM) on the RT1024 SDK, under "driver examples" > "ewm". Please let me know if this helps.
BR,
Edwin.
Hi @EdwinHz
Thanks for the response, Edwin.
Can i connect watch dog timer (TPS3850H01DRCT like externally) to the POR pin?
Yes, you should be able to connect the output of your external watchdog timer to the POR pin.
However, from the TPS3850H01DRCT datasheet, I see that the recommendation is to connect it to a NMI pin, so I suggest doing it this way instead.
BR,
Edwin.
Hi @EdwinHz ,
Based on your response, I understand that TPS3850H01DRCT (WDO) can be connected to the POR pin which is also a non-maskable interrupt pin (NMI) of MIMXRT1024CAG4B. Is my understanding correct?