EVK-MIMXRT685: I3C specification version

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

EVK-MIMXRT685: I3C specification version

Jump to solution
663 Views
Srukonja
Contributor III

Dear all,

I ran through the RT6xx- Reference Manual but wasn't able to find what I am looking for. Please share this information with me.

1) Which version of the MIPI I3C specification is supported by the RT6xx chip?

2) Which of the time-stamping mods (4 possible in total) are available on the RT6xx chip?

FYI this is the only information in the datasheet: A time-stamping option allows the resolution of an initial event, not just when an interrupt gets through. (pg. 570/1516)

Thanks in advance!

0 Kudos
1 Solution
650 Views
Alexis_A
NXP TechSupport
NXP TechSupport

Hello @Srukonja,

1.- The version is MIPI I3C v1.0 and I3C BasicSM v1.0

2.- The only time control available is Async Mode 0.

Best Regards,

Alexis Andalon

View solution in original post

1 Reply
651 Views
Alexis_A
NXP TechSupport
NXP TechSupport

Hello @Srukonja,

1.- The version is MIPI I3C v1.0 and I3C BasicSM v1.0

2.- The only time control available is Async Mode 0.

Best Regards,

Alexis Andalon