ECC check and inline encryption engine for SDRAM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

ECC check and inline encryption engine for SDRAM

跳至解决方案
1,907 次查看
Nagaveni
Contributor II

Hi,

 We are using IMXRT1170 EVK , could you please share and guide how to do ECC check for SDRAM and Inline encryption engine enabling to read and write data to  SDRAM.

Thanks in advance,

1 解答
1,894 次查看
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello
I hope you are well.

You can check this application note as well as this blog, although it is in Chinese it can be translated and contains helpful information:
-i.MX RT1170 ECC Application (nxp.com)
-痞子衡嵌入式:简析i.MXRT1170 XECC功能特点及其保护串行NOR Flash和SDRAM之道 - 痞子衡 - 博客园 (cnblogs.com)

Additionally, you might check the SDK examples as a reference for ECC and IEE.

If you have more questions do not hesitate to ask me.
Best regards,
Omar

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,895 次查看
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello
I hope you are well.

You can check this application note as well as this blog, although it is in Chinese it can be translated and contains helpful information:
-i.MX RT1170 ECC Application (nxp.com)
-痞子衡嵌入式:简析i.MXRT1170 XECC功能特点及其保护串行NOR Flash和SDRAM之道 - 痞子衡 - 博客园 (cnblogs.com)

Additionally, you might check the SDK examples as a reference for ECC and IEE.

If you have more questions do not hesitate to ask me.
Best regards,
Omar

0 项奖励
回复