Does the 'i.MX RT Series Crossover MCUs' 'Key Features' table need a review?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does the 'i.MX RT Series Crossover MCUs' 'Key Features' table need a review?

735 Views
rshipman
Contributor V

https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/i.mx-rt-series:IMX...

The 'i.MX RT Series Crossover MCUs' 'Key Features' table found at:

i.MX RT Series: MCU/Applications Crossover Processor | Arm® Cortex®-M7 | NXP 

says the RT1020 is at 600Mhz, but the document:

'i.MX RT1020 Processor Reference Manual, Rev. 1, 12/2018'

refers to a 500Mhz clock from the main PLL, although there are other PLLs, but none providing 600MHz that I can see.

Also if you click on the RT1020 link in the table, the blurb says "The i.MX RT1020 runs on the Arm® Cortex®-M7 core at 500 MHz."

So there you have it. Table is wrong.

Labels (1)
Tags (2)
0 Kudos
Reply
1 Reply

676 Views
jeremyzhou
NXP Employee
NXP Employee

Hi ,

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
After checking, the RT1020 can't run at 600 MHz actually, I think it's a typo on the website.

pastedImage_1.png

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply