Do you have an example of an RT1021 Flexio and edma driver camera?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Do you have an example of an RT1021 Flexio and edma driver camera?

685 Views
work2
Contributor I

Do you have an example of an RT1021 Flexio and edma driver camera?

I need to use edma to driver a camera, and I saw a chapter called "FlexIO Camera Driver" in the API Reference Manual. However, I can't really find it in the SDK package. MCUXpresso SDK API Reference Manual: FlexIO Camera Driver 

If you have the example or devices driver file, could you please send a copy to me? Thanks.

Labels (1)
Tags (2)
0 Kudos
1 Reply

491 Views
miduo
NXP Employee
NXP Employee

Hello,

Well, the sample driver you quoted is really for Kinetis family.  For RT family, we recommend RT1050 which has dedicate camera interface(CSI).

0 Kudos