Determining what boot mode proc expects

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Determining what boot mode proc expects

670 Views
jautry
Contributor IV

Is there a way to read the BOOT-MODE register to find out what the proc is set up for?  Trying to bring up new system and it appears to be in some other mode.  I did not see a reference to the address of this register in the reference manual.  Also, is it possible to tell if the eFuses are blown?

Tags (1)
0 Kudos
1 Reply

657 Views
jeremyzhou
NXP Employee
NXP Employee

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Is there a way to read the BOOT-MODE register to find out what the proc is set up for?
-- The Boot Mode register (SBMR), contains bits that reflect the status of Boot Mode Pins of the chip. The default values for those bits depend on the values of pins/fuses during the reset sequence, hence the question mark on their default value.
2) is it possible to tell if the eFuses are blown?
-- I'd highly recommend you to use the MCUXpresso Secure Provisioning tool to read eFuse to check whether some bits are blown.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos