Demo about FlexIO Shifter on Logic Mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Demo about FlexIO Shifter on Logic Mode

532 Views
kenmux
Contributor I

These days I struggled in using FlexIO shifter on logic mode.

Is there any demo for this?

I worked on the IMXRT1050-EVKB board.

Labels (2)
0 Kudos
1 Reply

462 Views
Sabina_Bruce
NXP Employee
NXP Employee

Hello ,

Hope you are doing well.

The examples that are available are under the section of FlexIO of the SDK. Here you will find a variety of examples, in addition some may use the shifter of this module. 

To learn more about the FLEXIO module please check these two posts.

Understanding FlexIO 

Introduction to FlexIO 

Best Regards,

Sabina

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

----------------------------------------------------------------------------------------------------------------------- 

0 Kudos