DMA controller uses the APBH bus

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DMA controller uses the APBH bus

843 Views
danbocko
Contributor I

Anyone have examples or starter code for the I.MX287 to use SSP with the DMA controller and the APBH bus. I am trying to read an 8-channel ADC and store the values using DMA. Working in RTOS instead of Linux.

Thanks

Dan

Tags (2)
0 Kudos
1 Reply

703 Views
igorpadykov
NXP Employee
NXP Employee

Hi Dan

unfortunately I am not aware of i.MX28 spi baremetal examples, may be useful to

check uboot patch on:

How to enable SPI NOR boot for i.MX28 (Spansion s25fl256s) 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos