Compatibility of different Arduino shields

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Compatibility of different Arduino shields

Jump to solution
939 Views
nilz
Contributor II

Hi,

Is the SparkFun Qwiic Shield for Arduino (https://www.sparkfun.com/products/14352) and Grid-EYE® Infrared (IR) Array Sensor Evaluation Kit (https://industry.panasonic.eu/components/sensors/grid-eye/grid-eye-evaluation-kit ) are compatible with NXP i.MX RT1010 Evaluation Kit (https://www.nxp.com/design/development- ... RT1010-EVK)?

Thanks in advance.

Labels (1)
0 Kudos
1 Solution
925 Views
Sabina_Bruce
NXP Employee
NXP Employee

Hello ,

Hope you are doing well.

I'd recommend to check the pin layout of both of those devices to make sure  they can be connected directly to the board using the headers. In addition, from checking the protocols used I don't see that you should have any problem using them with the RT1010. However, please consider that the implementation may have to be custom made in the application. As we do not have examples for these directly. 

Best Regards,

Sabina
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
926 Views
Sabina_Bruce
NXP Employee
NXP Employee

Hello ,

Hope you are doing well.

I'd recommend to check the pin layout of both of those devices to make sure  they can be connected directly to the board using the headers. In addition, from checking the protocols used I don't see that you should have any problem using them with the RT1010. However, please consider that the implementation may have to be custom made in the application. As we do not have examples for these directly. 

Best Regards,

Sabina

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

----------------------------------------------------------------------------------------------------------------------- 

0 Kudos