Clock initialization for FlexSPI in SDK for RT1051

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Clock initialization for FlexSPI in SDK for RT1051

566 Views
mastupristi
Senior Contributor I

Hallo,

in the FlexSPI examples, in the SDK, the clock setting (for FlexSPI itself) is done outside the BOARD_BootClockRUN() function in the clock_config.c file. It is done in the flexspi_clock_init() function called just before FlexSPI initialization.
Why this?

Is it safe and reliable to do all the clock initialization (including FlexSPI) in BOARD_BootClockRUN()?

best regards

Max

Labels (1)
0 Kudos
1 Reply

484 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello,

Please refer to the same  thread as the link. URL:https://community.nxp.com/thread/500456. Hope it help you.


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos