Clarify: RT1052 ADC external inputs

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Clarify: RT1052 ADC external inputs

1,533件の閲覧回数
bw1
Contributor IV

The reference manual IMXRT1050RM.pdf states in CH 14: "• Up to 8 single-ended external analog inputs".  However, it appears that more than that are mapped in section "14.2 External Signals".  Also, I am able to assign more than eight when using the Pins Tool (v3.0).  Can you please clarify how many external inputs we can actually connect to ADC inputs via physical pins of the part? 

ラベル(1)
タグ(1)
0 件の賞賛
1 返信

1,251件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Brad

there are 16 inputs described in Table 4-1. Muxing Options,
sect.14.2 External Signals i.MX RT1050 Reference Manual,

selected by register ADCx_HC0, ADCH: 00000-01111 External channels 0 to 15.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛