Can you save code to QSPI Flash?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can you save code to QSPI Flash?

Jump to solution
1,089 Views
bcstewart
Contributor III

The MIMXRT1010 looks intriguing.  The dev kit price is right ($10).

The demos are simple.  But does code go to SRAM?  Can you download code into the QSPI Flash?  If so, can you debug it?

Labels (1)
1 Solution
954 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,

Thanks for your reply.
1) Can I still do this on my own design using a J-Link or MultiLink SWD JTAG debugger?
-- Yes.
2) Can I mix data and code on the same QSPI Flash device?
-- Yes, of course.

TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

3 Replies
954 Views
jeremyzhou
NXP Employee
NXP Employee

Hi ,

Thank you for your interest in NXP Semiconductor products and the opportunity to serve you.
1) But does code go to SRAM?  
-- In the SDK library, the demos project not only allows you to debug it in the RAM but also in the QSPI flash just like the below figure shows.

pastedImage_1.png

TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
954 Views
bcstewart
Contributor III

That is good news.

Two more questions:

1.  Can I still do this on my own design using a J-Link or MultiLink SWD JTAG debugger?

2.  Can I mix data and code on the same QSPI Flash device?

Thank you,

Brad

0 Kudos
955 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,

Thanks for your reply.
1) Can I still do this on my own design using a J-Link or MultiLink SWD JTAG debugger?
-- Yes.
2) Can I mix data and code on the same QSPI Flash device?
-- Yes, of course.

TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------