Can we boot 1062 from FlexSPI2?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can we boot 1062 from FlexSPI2?

769 Views
MikeAitchison
Contributor I

We have (possibly mistakenly) connected our QSPI NOR to FlexSPI2. Can we use FlexSPI2 to connect to a boot device?

0 Kudos
1 Reply

750 Views
Sabina_Bruce
NXP Employee
NXP Employee

Hello Mike,

Hope you are doing well.

The i.MXRT1062 has two flexspi modules. The first one is used for booting only and the second can be used for a different purpose. The bootROM initializes certain modules and this includes FLEXSPI for booting. You may refer to the table provided in the boot chapter for all modules activated by bootROM in  section 9.5.2.

Best Regards,

Sabina

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

----------------------------------------------------------------------------------------------------------------------- 

0 Kudos