Hi All,
IDE:MCUXpresso IDE v11.3.0_5222
SDK:SDK_2.9.0_EVK-MIMXRT685
Sample Code: AN12796SW
Host: MIMXRT685-EVK
Slave: ICM-42605
Question1: I use your sample code to communicate with ICM-42605 in SDR mode. It can work. I want to try to use HDR-DDR mode that communicates with ICM-42605. Does it can work in this SDK? (or release the new sample code to support HDR-DDR mode)
Question2: Do you try to communicate with ICM-42605 in HDR-DDR mode? Can it work?
Thank-you for the support
Hello
Hope you are well.
HDR-DDR mode is supported in the RT600 I3C module. I suggest you update to the most recent SDK version(v2.10.1): https://mcuxpresso.nxp.com/en/welcome
Unfortunately, there is no specific example to enable HDR-DDR mode but the SDK has the functions to do it.
If you have more questions do not hesitate to ask me.
Best regards,
Omar