I am using MCUXpresso with the i.MXRT1064 evaluation kit.
There is an SDK example called `evkmimxrt1064_lpspi_interrupt_b2b_master` which uses LPSPI (specifically LPSPI1.)
I don't have two boards, so instead I hooked up a logic analyzer. At this point, I just want to see the signals change state. The LPSPI master should be able to drive Chip Select low even if a slave isn't physically present.
When the example runs, the logic analyzer sees no activity on any of the four signals.
The i.MXRT1064 EVK brings `GPIO_SD_B0_00 - GPIO_SD_B0_03` out to J24 positions 6,3,4,5. To set up IOMUX control to use the above pins: IOMUXC_SetPinMux( IOMUXC_GPIO_SD_B0_00_LPSPI1_SCK, /* GPIO_SD_B0_00 is configured as LPSPI1_SCK */ 0U); /* Software Input On Field: Input Path is determined by functionality */ IOMUXC_SetPinMux( IOMUXC_GPIO_SD_B0_01_LPSPI1_PCS0, /* GPIO_SD_B0_01 is configured as LPSPI1_PCS0 */ 0U); /* Software Input On Field: Input Path is determined by functionality */ IOMUXC_SetPinMux( IOMUXC_GPIO_SD_B0_02_LPSPI1_SDO, /* GPIO_SD_B0_02 is configured as LPSPI1_SDO */ 0U); /* Software Input On Field: Input Path is determined by functionality */ IOMUXC_SetPinMux( IOMUXC_GPIO_SD_B0_03_LPSPI1_SDI, /* GPIO_SD_B0_03 is configured as LPSPI1_SDI */ 0U); /* Software Input On Field: Input Path is determined by functionality */ Trying different pad configurations (pull up, drive strength) didn't make a difference.
I think I am missing something basic! Any advice appreciated.
Nik
解決済! 解決策の投稿を見る。
Hi Nicholas Langrind ,
Do you weld 0 ohm resistor to R278, R279,R280,R281?
Where is the test point you have connected to your logic analyzer ?
No signal, should be caused by no connection to the RT chip related pins.
Wish it helps you!
Kerry
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi Nicholas Langrind ,
Do you weld 0 ohm resistor to R278, R279,R280,R281?
Where is the test point you have connected to your logic analyzer ?
No signal, should be caused by no connection to the RT chip related pins.
Wish it helps you!
Kerry
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi Kerry,
I did not look see the DNP on the schematic. This is the explanation. Thanks very much.
(Hmm... I didn't read the example's documentation closely enough either. My bad.)
All the best,
Nik