Can I use external Static RAM with i.MXRT1050? I need more Static RAM with battery backup

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can I use external Static RAM with i.MXRT1050? I need more Static RAM with battery backup

1,033 Views
Soos
Contributor II

Is it possible to use external static RAM with iMXRT1050 ?

I need more battery backed-up RAM for our application.

Tags (1)
2 Replies

927 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

  The SEMC of the RT1050 supports devices with general purpose SRAM-like
interface.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

927 Views
Soos
Contributor II

OK Thanks

I will use SEMC_CSX0 as CS for my Static RAM.