Can I put Ethernet descriptors and buffers in OCRAM?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can I put Ethernet descriptors and buffers in OCRAM?

Jump to solution
1,662 Views
EdSutter
Senior Contributor II

Hi,

In the application examples from the SDK, it seems they all put Ethernet buffers/descriptors into DTCM. 

I'm using a '1062, so I'd like to relocate these buffers to OCRAM2 (using MPU to mark the portion of OCRAM2 used as non-cacheable/unbuffered).  This allows me to maximize the size of I/DTCM space.

I have not been able to get this to work.  Whenever I put the Ethernet buffers in OCRAM2 (non-cacheable/unbuffered) my network connection is unreliable.

Am I just configuring something wrong, or do I have to keep Ethernet buffers in DTCM space?

Tx 

Labels (1)
Tags (3)
0 Kudos
1 Solution
1,573 Views
EdSutter
Senior Contributor II

Thanks for the suggestions... I was doing that all along, the only change I made was to use OCRAM2 instead of DTCM.  That caused my driver to malfunction (drop packets), and that led me to the incorrect conclusion that for some reason I could not use OCRAM2 for Ethernet buffer descriptors.

Anyway, I found the problem... I had omitted the call to __DSB() just prior to writing to ENET->TDAR.

While I don't have time to fully understand why, I can say that empirically this fixed my problem.

Sooner or later I'll read up on why the Data Synchronization Barrier was needed for OCRAM2 but not DTCM.  I'm sure TCM has something to do with it, but I can't confirm that at this point.

View solution in original post

0 Kudos
5 Replies
1,574 Views
EdSutter
Senior Contributor II

Thanks for the suggestions... I was doing that all along, the only change I made was to use OCRAM2 instead of DTCM.  That caused my driver to malfunction (drop packets), and that led me to the incorrect conclusion that for some reason I could not use OCRAM2 for Ethernet buffer descriptors.

Anyway, I found the problem... I had omitted the call to __DSB() just prior to writing to ENET->TDAR.

While I don't have time to fully understand why, I can say that empirically this fixed my problem.

Sooner or later I'll read up on why the Data Synchronization Barrier was needed for OCRAM2 but not DTCM.  I'm sure TCM has something to do with it, but I can't confirm that at this point.

0 Kudos
1,573 Views
EdSutter
Senior Contributor II

Any other thoughts on this?  Seems to be a simple enough question...

Should I be able to locate the buffers and buffer-descriptors for ENET driver in OCRAM (0x20280000) or OCRAM2 (0x20200000)?  If yes, are there any working examples of this?

0 Kudos
1,573 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi Ed:

OCRAM can be config as non-cache region.  But I would suggest put critical code and data into TCM. Which is the fastest way for CPU to access the code and data.

Sorry there is not a demo for this.

You can refer to AN12042 for details.

pastedImage_1.png

Regards

Daniel 

0 Kudos
1,573 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi Ed:

Please make below change to set ENET data buffer memory location and try it again.

 

Original definition:(enet_ethernetif_kinetis.c)

    SDK_ALIGN(static rx_buffer_t rxDataBuff_0[ENET_RXBD_NUM], FSL_ENET_BUFF_ALIGNMENT);

    SDK_ALIGN(static tx_buffer_t txDataBuff_0[ENET_TXBD_NUM], FSL_ENET_BUFF_ALIGNMENT);

 

Change to:

  AT_NONCACHEABLE_SECTION_ALIGN(static rx_buffer_t rxDataBuff_0[ENET_RXBD_NUM], FSL_ENET_BUFF_ALIGNMENT);

  AT_NONCACHEABLE_SECTION_ALIGN(static tx_buffer_t txDataBuff_0[ENET_TXBD_NUM], FSL_ENET_BUFF_ALIGNMENT);

Regards

Daniel

0 Kudos
1,573 Views
EdSutter
Senior Contributor II

Thanks for responding, but I'm using that now ...

The SDK_ALIGN macro doesn't force the buffers anywhere, so using AT_NONCACHEABLE_SECTION_ALIGN

puts them in the same "NonCacheable" area as the buffer descriptors.  I made that change a while back.

But the linker file is what determines what memory space the NonCacheable section is placed in.

In the linker files under the lwip_examples directory, they put NonCacheable in either SDRAM or DTCM.

On my MIMX1060EVK eval board I've run with the same code but the linker file maps it to SDRAM and that works fine.

My custom hardware doesn't have SDRAM, and the Ethernet driver runs fine as long as I have NonCacheable mapped into DTCM.  I'd like to have theses buffers in OCRAM2 if possible, so my question stands...

  

MEMORY

{

...

  m_data                (RW)  : ORIGIN = 0x20000000, LENGTH = 0x00020000

...

}

SECTIONS

{

....

   .ncache :
   {
   *(NonCacheable)
   . = ALIGN(4);
   __noncachedata_end__ = .;
   } > m_data

...

}

All I'd like to be able to do is change the ORIGIN to 0x20200000 (OCRAM2), and use the MPU to make

that space non-cacheable.  Should I be able to do that?

0 Kudos