Can I.MX RT1050 XIP from encrypted parallel nor?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can I.MX RT1050 XIP from encrypted parallel nor?

Jump to solution
1,533 Views
loverdeg
Contributor II

Can I.MX RT1050 XIP from encrypted parallel nor?

I'm assuming not considering I see no mention of it in any documentation.

Also what sort of performance bottle-neck would be seen with XIP from parallel flash? (encrypted or not)

How does this bottleneck compare to XIP from ultraflash or qpsi flash?

Labels (1)
1 Solution
1,297 Views
343mjt
Contributor II

Hi Artur,

What other options are there for encrypted XiP support through means other than FlexSPI/serial NOR flash?

Thanks

Matt

View solution in original post

3 Replies
1,297 Views
jay_heng
NXP Employee
NXP Employee

You can also try this tool, with this tool, You can flash bare image into various boot devices easily and don't need to care about headers (ivt, boot data...)

GitHub - JayHeng/nxp-sec-boot-ui: A one-stop GUI tool to work with NXP MCU (Kinetis, i.MXRT, LPC) RO... 

0 Kudos
1,297 Views
art
NXP Employee
NXP Employee

No, there is no encrypted XiP support for parallel NOR Flash. The encrypted XiP is only supported for serial NOR Flash via the FlexSPI interface.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
1,298 Views
343mjt
Contributor II

Hi Artur,

What other options are there for encrypted XiP support through means other than FlexSPI/serial NOR flash?

Thanks

Matt