Camera Application with i.MX RT1050

cancel
Showing results for 
Search instead for 
Did you mean: 

Camera Application with i.MX RT1050

Jump to solution
362 Views
tomars
Contributor II

Hello!

I found this document:

https://www.nxp.com/docs/en/application-note/AN12110.pdf 

Really nice example!

i looking for the code for this example. Is it available?(incorporated camera, sd card and lcd)

Best regards!

Labels (1)
1 Solution
236 Views
jeremyzhou
NXP TechSupport
NXP TechSupport

Hi ,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
There's no similar the code for the application note, the application note proposes the developer to follow the step which is demonstrated in the application note to create the Camera Application project, and in my opinion, it's equal to integrating the sd_jpeg and rgb565 demos which are from the SDK library.
Hope this is clear.

TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

2 Replies
237 Views
jeremyzhou
NXP TechSupport
NXP TechSupport

Hi ,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
There's no similar the code for the application note, the application note proposes the developer to follow the step which is demonstrated in the application note to create the Camera Application project, and in my opinion, it's equal to integrating the sd_jpeg and rgb565 demos which are from the SDK library.
Hope this is clear.

TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

236 Views
tomars
Contributor II

Yes, thank You!

I will use those examples.

0 Kudos