Boot from SD in i.MXRT1050

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Boot from SD in i.MXRT1050

1,879 Views
rans
Senior Contributor I

Hello,

I hope someone can help me understand booting from sd as described in :

https://www.nxp.com/docs/en/application-note/AN12107.pdf 

I see that the .bd file uses offset 0x0000a0000 in page 28:

"Step 3: Find the linkfile MIMXRT1052xxxxx_ram.icf and change the start vector table from 0x0000A000."

I see in memory map that it is inside ITCM:

0000_0000 0007_FFFF 512KB ITCM

 But what is the purpose of offset 0xa000 inside ?

Thank you,

ranran

2 Replies

1,429 Views
igorpadykov
NXP Employee
NXP Employee

Hi ranran

" 0xa000" seems as misrpint, one can refer to p.22 attached document.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,429 Views
asick
Contributor III

Demo application running successfully through SD card boot !

I have doubt on, through Serial download mode where image file got placed & Which partition SD card ?

0 Kudos