Hello,
I hope someone can help me understand booting from sd as described in :
https://www.nxp.com/docs/en/application-note/AN12107.pdf
I see that the .bd file uses offset 0x0000a0000 in page 28:
"Step 3: Find the linkfile MIMXRT1052xxxxx_ram.icf and change the start vector table from 0x0000A000."
I see in memory map that it is inside ITCM:
0000_0000 0007_FFFF 512KB ITCM
But what is the purpose of offset 0xa000 inside ?
Thank you,
ranran
Hi ranran
" 0xa000" seems as misrpint, one can refer to p.22 attached document.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Demo application running successfully through SD card boot !
I have doubt on, through Serial download mode where image file got placed & Which partition SD card ?