Boot RT1062 from IS25LP512M-JLLE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Boot RT1062 from IS25LP512M-JLLE

1,003 Views
paul_brandt
Contributor I

Hi,

on the RT1060 EVK we have the option to boot from the onboard IS25WP064AJBLE.
In our custom design we have to use a higher capacity and 3.3V QSPI Flash to boot from.
We decided to take the IS25LP512M-JLLE as it comes the closest to the IS25WP064AJBLE on the EVK.
This is how it is connected to the RT1062.
Bildschirmfoto 2019-12-09 um 13.14.33.png
Bildschirmfoto 2019-12-09 um 13.13.23.png

Q: Will we be able to boot from it and what will be needed actions for that?

Thank you very much!
Paul

Labels (1)
Tags (2)
2 Replies

842 Views
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Paul Brandt

Yes, there shouldn't be any problem to use this memory with those capacitor value and the voltage level. In order to be able to use this memory, you need to change the driver used to program it and in the SDK software, in the xip folder, change the configurations that are defined for the EVK board.

Hope this helps.

Best regards

Jorge Alcala

0 Kudos

842 Views
nxp16
Contributor III

Hi,

We're trying to use a similar flash chip, IS25LP128-JKLE.  We can't get it to flash.  Can you tell me what we need to change the driver to and what we have to do for configuration in the xip folder?

Thanks,

-m