Hi All,
I was trying to analyze performance of OTFAD & IEE decryption module.
From application note "AN13198" i can able to find sample code to check OTFAD performance, but I couldn't able to find OTFAD configurations which is used by "BOOTROM" for decryption.
Where can i find the configuration details for OTFAD & IEE decryption.
PS: like AN13198 is there any application note available for IEE decryption sample code?
Regards,
Sathishkumar K
iMXRT1160
Hi @sathishkumar-rk ,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Where can i find the configuration details for OTFAD & IEE decryption?
-- To provide the fastest support, please refer to the application note.
2) like AN13198 is there any application note available for the IEE decryption sample code?
-- The source code is also suitable for testing the performance of the IEE encryption mode.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------f