BOOT_CFG2[2:0] settings for IMXRT1170 FlexSPI Serial NOR boot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

BOOT_CFG2[2:0] settings for IMXRT1170 FlexSPI Serial NOR boot

Jump to solution
991 Views
takayuki_ishii
Contributor IV

Hello community,

 

I have one question about BOOT_CFG2[2:0]=000 bit setting for IMXRT1170.

In Reference Manual for IMXRT1050, it have more information about BOOT_CFG2[2:0].

takayuki_ishii_0-1646113817368.png

But Reference manual for IMXRT1170 have only minimal information.

takayuki_ishii_1-1646113889725.png

Is BOOT_CFG2[2:0]=000b setting is same as RT1050?

 

I look forward to hearing from you.

 

Best regards,

Ishii.

 

Tags (1)
0 Kudos
1 Solution
985 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1)Is BOOT_CFG2[2:0]=000b setting is same as RT1050?
-- Yes, they're almost the same.
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
2 Replies
986 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1)Is BOOT_CFG2[2:0]=000b setting is same as RT1050?
-- Yes, they're almost the same.
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
982 Views
takayuki_ishii
Contributor IV

Hello @jeremyzhou 

 

Thank you for your quick reply.

I will answer it to my customer.

 

Best regards,

Ishii.

 

0 Kudos