About low power mode on mxrt1021

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About low power mode on mxrt1021

620 Views
hiro8235
Contributor I

Can the low power mode be enabled with an empty ROM?
If so, is there a description of the settings in the IMXRT1021RM?
For example, system idle mode settings.
Thank you.

Labels (1)
0 Kudos
3 Replies

614 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @hiro8235 

   low power mode enter need to use the code, you can download it to the internal RAM instead of the external flash, I think your mentioned empty ROM is no code in the external flash, right?

   If yes, you can download this SDK code to the RAM, just not do the POR, the low power code will help you enter the low power mode.

\SDK_2_11_0_EVK-MIMXRT1020\boards\evkmimxrt1020\demo_apps\power_mode_switch

SDK download link is:

https://mcuxpresso.nxp.com/en/builder?hw=EVK-MIMXRT1020

 

Wish it helps you!

Best Regards,

Kerry

0 Kudos

612 Views
hiro8235
Contributor I

Hi Kerry.

Thank you for your reply.
OK, I will try to SDK code to the RAM.

Best Regards,

Hiro

0 Kudos

609 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @hiro8235 

  You are welcome!

   If you meet any issues, just let me know.

  If your question is solved, please help to mark the correct answer, just to close this case, any new issues, welcome to create the new question post!

 

Best Regards,

kerry

0 Kudos