Hi,
I am using IMXRT1170 board and getting bus fault while running my application with debug log error A precise data access error has occurred (CFSR.PRECISERR, BFAR)
please find the below Debug log for information
Wed Sep 27, 2023 12:41:44: IAR Embedded Workbench 9.30.1 (C:\Program Files\IAR Systems\Embedded Workbench 9.1_2\arm\bin\armPROC.dll)
Wed Sep 27, 2023 12:41:44: Loaded macro file: C:\Program Files\IAR Systems\Embedded Workbench 9.1_2\arm/config/debugger/NXP/iMXRT_1170.dmac
Wed Sep 27, 2023 12:41:44: Loaded macro file: C:\Program Files\IAR Systems\Embedded Workbench 9.1_2\arm/config/debugger/NXP/iMXRT_1170_cm7.dmac
Wed Sep 27, 2023 12:41:44: Loaded macro file: C:\Program Files\IAR Systems\Embedded Workbench 9.1_2\arm/config/flashloader/NXP/FlashIMXRT1170_FlexSPI.mac
Wed Sep 27, 2023 12:41:45: JLINK command: ProjectFile = D:\Git_13092023\TE_01_Baxter_Doppler_Monitor\IMXRT117x_Software\Application\IAR_Project\settings\IAR_Project_flexspi_nor_debug.jlink, return = 0
Wed Sep 27, 2023 12:41:45: Device "MIMXRT1176XXXA_M7" selected.
Wed Sep 27, 2023 12:41:45: DLL version: V7.66 , compiled May 18 2022 15:57:48
Wed Sep 27, 2023 12:41:45: Firmware: J-Link V11 compiled May 23 2023 14:44:38
Wed Sep 27, 2023 12:41:45: Selecting SWD as current target interface.
Wed Sep 27, 2023 12:41:45: JTAG speed is initially set to: 32 kHz
Wed Sep 27, 2023 12:41:45: Found SW-DP with ID 0x6BA02477
Wed Sep 27, 2023 12:41:45: DPIDR: 0x6BA02477
Wed Sep 27, 2023 12:41:45: CoreSight SoC-400 or earlier
Wed Sep 27, 2023 12:41:45: Scanning AP map to find all available APs
Wed Sep 27, 2023 12:41:45: AP[1]: Stopped AP scan as end of AP map has been reached
Wed Sep 27, 2023 12:41:45: AP[0]: AHB-AP (IDR: 0x84770001)
Wed Sep 27, 2023 12:41:45: Iterating through AP map to find AHB-AP to use
Wed Sep 27, 2023 12:41:46: AP[0]: Core found
Wed Sep 27, 2023 12:41:46: AP[0]: AHB-AP ROM base: 0xE00FD000
Wed Sep 27, 2023 12:41:46: CPUID register: 0x411FC272. Implementer code: 0x41 (ARM)
Wed Sep 27, 2023 12:41:46: Found Cortex-M7 r1p2, Little endian.
Wed Sep 27, 2023 12:41:46: FPUnit: 8 code (BP) slots and 0 literal slots
Wed Sep 27, 2023 12:41:46: CoreSight components:
Wed Sep 27, 2023 12:41:46: ROMTbl[0] @ E00FD000
Wed Sep 27, 2023 12:41:46: [0][0]: E00FE000 CID B105100D PID 000BB4C8 ROM Table
Wed Sep 27, 2023 12:41:46: ROMTbl[1] @ E00FE000
Wed Sep 27, 2023 12:41:46: [1][0]: E00FF000 CID B105100D PID 000BB4C7 ROM Table
Wed Sep 27, 2023 12:41:46: ROMTbl[2] @ E00FF000
Wed Sep 27, 2023 12:41:46: [2][0]: E000E000 CID B105E00D PID 000BB00C SCS-M7
Wed Sep 27, 2023 12:41:46: [2][1]: E0001000 CID B105E00D PID 000BB002 DWT
Wed Sep 27, 2023 12:41:46: [2][2]: E0002000 CID B105E00D PID 000BB00E FPB-M7
Wed Sep 27, 2023 12:41:46: [2][3]: E0000000 CID B105E00D PID 000BB001 ITM
Wed Sep 27, 2023 12:41:46: [1][1]: E0041000 CID B105900D PID 001BB975 ETM-M7
Wed Sep 27, 2023 12:41:46: [1][2]: E0042000 CID B105900D PID 004BB906 CTI
Wed Sep 27, 2023 12:41:46: [0][1]: E0043000 CID B105900D PID 001BB908 CSTF
Wed Sep 27, 2023 12:41:46: Cache: Separate I- and D-cache.
Wed Sep 27, 2023 12:41:46: I-Cache L1: 32 KB, 512 Sets, 32 Bytes/Line, 2-Way
Wed Sep 27, 2023 12:41:46: D-Cache L1: 32 KB, 256 Sets, 32 Bytes/Line, 4-Way
Wed Sep 27, 2023 12:41:46: Reset: Halt core after reset via DEMCR.VC_CORERESET.
Wed Sep 27, 2023 12:41:46: Reset: Reset device via AIRCR.SYSRESETREQ.
Wed Sep 27, 2023 12:41:46: AfterResetTarget() start
Wed Sep 27, 2023 12:41:46: Valid application detected. Setting PC / SP manually.
Wed Sep 27, 2023 12:41:46: PC = 0x30007125
Wed Sep 27, 2023 12:41:46: SP = 0x20040000
Wed Sep 27, 2023 12:41:46: Clean & invalidate cached CPU registers
Wed Sep 27, 2023 12:41:46: AfterResetTarget() end
Wed Sep 27, 2023 12:41:47: Hardware reset with strategy 0 was performed
Wed Sep 27, 2023 12:41:47: Initial reset was performed
Wed Sep 27, 2023 12:41:49: Loaded debugee: C:\Program Files\IAR Systems\Embedded Workbench 9.1_2\arm/config/flashloader/NXP/FlashIMXRT1170_FlexSPI.out
Wed Sep 27, 2023 12:41:49: Target reset
Wed Sep 27, 2023 12:42:12: Unloaded macro file: C:\Program Files\IAR Systems\Embedded Workbench 9.1_2\arm/config/flashloader/NXP/FlashIMXRT1170_FlexSPI.mac
Wed Sep 27, 2023 12:42:12: Downloaded D:\Git_13092023\TE_01_Baxter_Doppler_Monitor\IMXRT117x_Software\Application\IAR_Project\flexspi_nor_debug\lwip_dhcp_usb_freertos.out to flash memory.
Wed Sep 27, 2023 12:42:12: 849020 bytes downloaded into FLASH (29.17 Kbytes/sec)
Wed Sep 27, 2023 12:42:12: Loaded macro file: D:\Git_13092023\TE_01_Baxter_Doppler_Monitor\IMXRT117x_Software\Application\IAR_Project/evkmimxrt1170/evkmimxrt1170_connect_cm7.mac
Wed Sep 27, 2023 12:42:13: FlexRAM configuration is restored
Wed Sep 27, 2023 12:42:13: SDRAM init done
Wed Sep 27, 2023 12:42:21: Loaded debugee: D:\Git_13092023\TE_01_Baxter_Doppler_Monitor\IMXRT117x_Software\Application\IAR_Project\flexspi_nor_debug\lwip_dhcp_usb_freertos.out
Wed Sep 27, 2023 12:42:26: Reset: Halt core after reset via DEMCR.VC_CORERESET.
Wed Sep 27, 2023 12:42:26: Reset: Reset device via AIRCR.SYSRESETREQ.
Wed Sep 27, 2023 12:42:26: AfterResetTarget() start
Wed Sep 27, 2023 12:42:26: Valid application detected. Setting PC / SP manually.
Wed Sep 27, 2023 12:42:26: PC = 0x30007125
Wed Sep 27, 2023 12:42:26: SP = 0x20040000
Wed Sep 27, 2023 12:42:26: Clean & invalidate cached CPU registers
Wed Sep 27, 2023 12:42:26: AfterResetTarget() end
Wed Sep 27, 2023 12:42:26: Hardware reset with strategy 0 was performed
Wed Sep 27, 2023 12:42:26: 849020 bytes verified (154.66 Kbytes/sec)
Wed Sep 27, 2023 12:42:26: Download completed and verification successful.
Wed Sep 27, 2023 12:42:26: Reset: Halt core after reset via DEMCR.VC_CORERESET.
Wed Sep 27, 2023 12:42:26: Reset: Reset device via AIRCR.SYSRESETREQ.
Wed Sep 27, 2023 12:42:26: AfterResetTarget() start
Wed Sep 27, 2023 12:42:26: Valid application detected. Setting PC / SP manually.
Wed Sep 27, 2023 12:42:26: PC = 0x30007125
Wed Sep 27, 2023 12:42:26: SP = 0x20040000
Wed Sep 27, 2023 12:42:26: Clean & invalidate cached CPU registers
Wed Sep 27, 2023 12:42:26: AfterResetTarget() end
Wed Sep 27, 2023 12:42:26: Software reset was performed
Wed Sep 27, 2023 12:42:26: Target reset
Wed Sep 27, 2023 12:42:47: BusFault exception.
Wed Sep 27, 2023 12:42:47: A precise data access error has occurred (CFSR.PRECISERR, BFAR)
Wed Sep 27, 2023 12:42:47: At data address 0x86000000.
Wed Sep 27, 2023 12:42:47: An imprecise data access error has occurred (CFSR.IMPRECISERR, BFAR)
Wed Sep 27, 2023 12:42:47: At data address 0x86000000.
Wed Sep 27, 2023 12:42:47: Exception occurred at PC = 0x301b18a6, LR = 0x301b183b
Wed Sep 27, 2023 12:42:47: See the call stack for more information.
This address mentioned in linker file , Please find the attached linker file for More information. Particular __FILE_FIRMWARE_BUFFER__ only facing issue if I remove this application is working properly
please find the preprocessor in command line
__REDLIB__
SKIP_SYSCLK_INIT
CPU_MIMXRT1176DVMAA
CPU_MIMXRT1176DVMAA_cm7
DATA_SECTION_IS_CACHEABLE=1
_DEBUG=1
XIP_EXTERNAL_FLASH=1
XIP_BOOT_HEADER_ENABLE=0
XIP_BOOT_HEADER_DCD_ENABLE=1
USE_RTOS=1
USB_STACK_FREERTOS
PRINTF_ADVANCED_ENABLE=1
SDK_DEBUGCONSOLE=1
SERIAL_PORT_TYPE_UART=1
SDK_OS_FREE_RTOS
MCUXPRESSO_SDK
DEBUG
__USE_CMSIS
CR_INTEGER_PRINTF
PRINTF_FLOAT_ENABLE=1
SERIAL_PORT_TYPE_UART=1
_DLIB_FILE_DESCRIPTOR
USE_SDRAM
SDK_I2C_BASED_COMPONENT_USED
DEBUG_CONSOLE_RX_ENABLE=0
DEBUG_CONSOLE_TRANSFER_NON_BLOCKING
SHELL_NON_BLOCKING_MODE=1
SHELL_HANDLER_ENABLE=1
please let me know where I am missing ?
Thanks In Advance