16bit voice input from RT1170-EVK PDM microphones

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

16bit voice input from RT1170-EVK PDM microphones

Jump to solution
1,101 Views
yf2
Contributor III

Dear support,

 

Would you please teach how to efficiently get 16bit voice wave data from PDM microphones on RT1170-EVK device?

the MCUExpresso SDK defines data width for 24bit and 32bit when FSL_FEATURE_PDM_FIFO_WIDTH is set as (4), this is the case in my MIMXRT1176_cm7_features.h.

How can we do 16bit data capture via PDM driver on RT1170-EVK board? Do we have to capture in 24 or 32bit then convert to 16bit manually?

The old ticket1 and ticket2 will be closed to avoid duplications.

 

Regards,

yf2

Tags (2)
0 Kudos
1 Solution
1,089 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @yf2 ,

  From the RT1170 RM, it is 24 bit:

kerryzhou_0-1657273485852.png

Anyway, I will help you double check with our internal side, whether it can support 16 bit or not, then I will give you updated information.

Best Regards,

kerry

 

View solution in original post

0 Kudos
4 Replies
1,088 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @yf2 ,

   Please help to check one point, how many bit of your external mic? 16bit? signed?

   Please give me reply, then I will check with our expert again, thanks.

Best Regards,

Kerry

0 Kudos
1,074 Views
yf2
Contributor III

Kerry,

We cosulted contact of PDM microphone vendor and they said it is up to the PDM receiver side to decide the audio output data width. Some receivers may output 24bit, some may output 16bit.

So please kindly check with RT117x team and let me know what I can do with the microphone vendor.

Regards,

yf2

0 Kudos
1,071 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @yf2 ,

  I already get our internal expert reply: RT1170 PDM is 24 bit, but it also supports 16bit, when you want to use the 16 bit, just read the higher 16 bit in the get 24 bit data.

kerryzhou_0-1657527146203.png

 

Wish it helps you!

Best Regards,

Kerry

 

0 Kudos
1,090 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @yf2 ,

  From the RT1170 RM, it is 24 bit:

kerryzhou_0-1657273485852.png

Anyway, I will help you double check with our internal side, whether it can support 16 bit or not, then I will give you updated information.

Best Regards,

kerry

 

0 Kudos