i.MX RT Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX RT Knowledge Base

Labels

Discussions

Sort by:
LittleFS is a file system used for microcontroller internal flash and external NOR flash. Since it is more suitable for small embedded systems than traditional FAT file systems, more and more people are using it in their projects. So in addition to NOR/NAND flash type storage devices, can LittleFS be used in SD cards? It seems that it is okay too. This article will use the littlefs_shell and sdcard_fatfs demo project in the i.mxRT1050 SDK to make a new littefs_shell project for reading and writing SD cards. This experiment uses MCUXpresso IDE v11.7, and the SDK uses version 2.13. The littleFS file system has only 4 files, of which the current version shown in lfs.h is littleFS 2.5. The first step, of course, is to add SD-related code to the littlefs_shell project. The easiest way is to import another sdcard_fatfs project and copy all of the sdmmc directories into our project. Then copy sdmmc_config.c and sdmmc_config.h in the /board directory, and fsl_usdhc.c and fsl_usdhc.h in the /drivers directory. The second step is to modify the program to include SD card detection and initialization, adding a bridge from LittleFS to SD drivers. Add the following code to littlefs_shell.c. extern sd_card_t m_sdCard; status_t sdcardWaitCardInsert(void) { BOARD_SD_Config(&m_sdCard, NULL, BOARD_SDMMC_SD_HOST_IRQ_PRIORITY, NULL); /* SD host init function */ if (SD_HostInit(&m_sdCard) != kStatus_Success) { PRINTF("\r\nSD host init fail\r\n"); return kStatus_Fail; } /* wait card insert */ if (SD_PollingCardInsert(&m_sdCard, kSD_Inserted) == kStatus_Success) { PRINTF("\r\nCard inserted.\r\n"); /* power off card */ SD_SetCardPower(&m_sdCard, false); /* power on the card */ SD_SetCardPower(&m_sdCard, true); // SdMmc_Init(); } else { PRINTF("\r\nCard detect fail.\r\n"); return kStatus_Fail; } return kStatus_Success; } status_t sd_disk_initialize() { static bool isCardInitialized = false; /* demostrate the normal flow of card re-initialization. If re-initialization is not neccessary, return RES_OK directly will be fine */ if(isCardInitialized) { SD_Deinit(&m_sdCard); } if (kStatus_Success != SD_Init(&m_sdCard)) { SD_Deinit(&m_sdCard); memset(&m_sdCard, 0U, sizeof(m_sdCard)); return kStatus_Fail; } isCardInitialized = true; return kStatus_Success; } In main(), add these code if (sdcardWaitCardInsert() != kStatus_Success) { return -1; } status = sd_disk_initialize(); Next, create two new c files, lfs_sdmmc.c and lfs_sdmmc_bridge.c. The call order is littlefs->lfs_sdmmc.c->lfs_sdmmc_bridge.c->fsl_sd.c. lfs_sdmmc.c and lfs_sdmmc_bridge.c acting as intermediate layers that can connect the LITTLEFS and SD upper layer drivers. One of the things that must be noted is the mapping of addresses. The address given by littleFS is the block address + offset address. See figure below. This is a read command issued by the ‘mount’ command. The block address refers to the address of the erased sector address in SD. The read and write operation uses the smallest read-write block address (BLOCK) of SD, as described below. Therefore, in lfs_sdmmc.c, the address given by littleFS is first converted to the byte address. Then change the SD card read-write address to the BLOCK address in lfs_sdmmc_bridge.c. Since most SD cards today exceed 4GB, the byte address requires a 64-bit variable. Finally, the most important step is littleFS parameter configuration. There is a structure LittlsFS_config in peripherals.c, which contains not only the operation functions of the SD card, but also the read and write sectors and cache size. The setup of this structure is critical. If the setting is not good, it will not only affect the performance, but also cause errors in operation. Before setting it up, let's introduce some of the general ideal of SD card and littleFS. The storage unit of the SD card is BLOCK, and both reading and writing can be carried out according to BLOCK. The size of each block can be different for different cards. For standard SD cards, the length of the block command can be set with CMD16, and the block command length is fixed at 512 bytes for SDHC cards. The SD card is erased sector by sector. The size of each sector needs to be checked in the CSD register of the SD card. If the CSD register ERASE_BLK_EN = 0, Sector is the smallest erase unit, and its unit is "block". The value of sector size is equal to the value of the SECTOR_SIZE field in the CSD register plus 1. For example, if SECTOR_SIZE is 127, then the minimum erase unit is 512*(127+1)=65536 bytes. In addition, sometimes there are doubts, many of the current SD cards actually have wear functions to reduce the loss caused by frequent erasing and writing, and extend the service life. So in fact, delete operations or read and write operations are not necessarily real physical addresses. Instead, it is mapped by the SD controller. But for the user, this mapping is transparent. So don't worry about this affecting normal operation. LittleFS is a lightweight file system that has power loss recovery and dynamic wear leveling compared to FAT systems. Once mounted, littleFS provides a complete set of POSIX-like file and directory functions, so it can be operated like a common file system. LittleFS has only 4 files in total, and it basically does not need to be modified when used. Since the NOR/NAND flash to be operated by LittleFS is essentially a block device, in order to facilitate use, LittleFS is read and written in blocks, and the underlying NOR/NAND Flash interface drivers are carried out in blocks. Let's take a look at the specific content of LittleFS configuration parameters. const struct lfs_config LittleFS_config = { .context = (void*)0, .read = lfs_sdmmc_read, .prog = lfs_sdmmc_prog, .erase = lfs_sdmmc_erase, .sync = lfs_sdmmc_sync, .read_size = 512, .prog_size = 512, .block_size = 65536, .block_count = 128, .block_cycles = 100, .cache_size = 512, .lookahead_size = LITTLEFS_LOOKAHEAD_SIZE }; Among them, the first item (.context) is not used in this project, and is used in the original project to save the offset of the file system stored in Flash. Items two (.read) through five (.sync) point to the handlers for each operation. The sixth item (.read_size) is the smallest unit of read operation. This value is roughly equal to the BLOCK size of the SD card. In the SD card driver, this size has been fixed to 512. So for convenience, it is also set to 512. The seventh item (.prog_size) is the number of bytes written each time, which is 512 bytes like .read_size. The eighth item is .block_size. This can be considered to be the smallest erase block supported by the SD card when performing an erase operation. Here the default value is not important, you need to set it in the program according to the actual value after the SD card is initialized. The card used in this experiment is 64k bytes as an erase block, so 65536 is used directly here. Item 9 (.block_count) is used to indicate how many erasable blocks there are. Multiply the .block_size to get the size of the card. If the card is replaceable, it needs to be determined according to the parameters after the SD card is initialized. The tenth item (.block_cycles) is the number of erase cycles per block. Item 11 (.cache_size) is about the cache buffer. It feels like bigger is better, but actually modifies this value won't work. So still 512. Item 12 (lookahead_size), littleFS uses a lookahead buffer to manage and allocate blocks. A lookahead buffer is a fixed-size bitmap that records information about block allocations within an area. The lookahead buffer only records the information of block allocations in one area, and when you need to know the allocation of other regions, you need to scan the file system to find allocated blocks. If there are no free blocks in the lookahead buffer, you need to move the lookahead buffer to find other free blocks in the file system. The lookahead buffer position shifts one lookahead_size at a time. Use the original value here.  That’s all for the porting work. We can test the project now. You can see it works fine. The littleFS-SD project can read/write/create folder and erase. And it also support append to an exist file. But after more testing, a problem was found, if you repeatedly add->-close->-add-> close a file, the file will open more and more slowly, even taking a few seconds. This is what should be added and is not written directly in the last block of the file, but will apply for a new block, regardless of whether the previous block is full or not. See figure below. The figure above prints out all the read, write, and erase operations used in each write command. You can see that each time in the lfs_file_open there is one more read than the last write operation. In this way, after dozens or hundreds of cycles, a file will involve many blocks. It is very time-consuming to read these blocks in turn. Tests found that more than 100 read took longer than seconds. To speed things up, it is recommended to copy the contents of one file to another file after adding it dozens of times. In this way, the scattered content will be consolidated to write a small number of blocks. This can greatly speed up reading and writing.
View full article
Issue: 802.11 IEEE station Power Save mode is not working as expected with the latest SDK 2.11.1, supporting NXP wireless solutions 88W8987/88W8977/IW416.   Solution: Modify the structure in file : middleware/wifi/wifidriver/incl/mlan_fw.h, Replace  “ENH_PS_MODES action” to “uint16_t action”.    Note: This fix will officially be part of SDK: 2.12.0
View full article
RT600 MCUXpresso JLINK debug QSPI flash 1 Introduction     MIMXRT600-EVK is the NXP official board, which onboard flash is the external octal flash, the octal flash is connected to the RT685 flexSPI portB. In practical usage, the customer board may use other flash types, eg QSPI flash, and connect to the FlexSPI A port. Recently, nxp published one RT600 customer flash application note: https://www.nxp.com/docs/en/application-note/AN13386.pdf This document mainly gives the CMSIS DAP related flash algorithm usage, which modifies the option data to generate the new flash algo for the different flash types. Some customer’s own board may use the RT600 QSPI flash+MCUXPresso+JLINK to debug the application code. Recently, one of the customers find on his own customer board, when they use debugger JLINK associated with the MCUXPresso download code to the RT600 QSPI flash, they meet download issues, but when using the CMSIS DAP as a debugger and the related QSPI cfx file, they can download OK. So this document mainly gives the experience of how to use the RT600, MCUXpresso IDE, and JLINK to download and debug the code which is located in the external QSPI flash. 2 JLINK driver prepare and test   MCUXpresso IDE use the JLINK download, it will call the JLINK driver related script and the flash algorithm, but to RT600, the JLINK driver will use the RT600 EVK flexSPI port B octal flash in default, so, if the customer board changes to other flexSPI port and to QSPI flash, they need to provide the related QSPI flash algorithm and script file, otherwise, even they can find the ARM CM33 core, the download will be still failed. If customers want to use the MCUXpresso IDE and the JLINK, they need to make sure the JLINK driver attached tool can do the external flash operation, eg, erase, read, write successfully at first. Now, give the JLINK driver related tool how to add the RT600 QSPI flash driver and script file. 2.1 JLINK driver install   Download the Segger JLINK driver from the following link: https://www.segger.com/downloads/jlink/JLink_Windows_V754b_x86_64.exe This document will use the jlink v7.54b to test, other version is similar. Install the driver, the default driver install path is: C:\Program Files\SEGGER 2.2 Universal flashloader RT-UFL    RT-UFL v1.0 is a universal flashloader, which uses one .FLM file for all i.MXRT chips, and the different external flash, it is mainly used for the Segger JLINK debugger. RT-UFL v1.0 downoad link: https://github.com/JayHeng/RT-UFL/archive/refs/tags/v1.0.zip    Now, to the RT600 QSPI, give the related flash algo file patch.    Copy the following path file: \RT-UFL-1.0\algo\SEGGER\JLink_Vxxx To the JLINK install path: \SEGGER\JLink Then copy the content in file: RT-UFL-master\test\SEGGER\JLink_Vxxx\Devices\NXP\iMXRT6xx\archive2\evkmimxrt685.JLinkScript To replace the content in: C:\Program Files\SEGGER\JLink\Devices\NXP\iMXRT_UFL\iMXRT6xx_CortexM33.JLinkScript Otherwise, the MCUXpresso IDE debug reset button function will not work. So, need to add the JLINKScript code for ResetTarget, which will reset the external flash. pic1 The RT-UFL provide 3 types download flash algo: MIMXRT600_UFL_L0, MIMXRT600_UFL_L1, MIMXRT600_UFL_L2. Pic 2 _L0 used for the QSPI Flash and Octal Flash(page size 256 Bytes, sector size 4KB), _L1/2 used for the hyper flash(Page size 512 Bytes,Sector size 4KB/64KB). The JLINKDevices.xml content also can get the detail information. Different name will call different .FLM, the .FLM is the flash algorithm file, the source code can be found in RT-UFL v1.0, it will use different option0 option1 to configure the different external memory when the memory chip can support SFDP. <Device> <ChipInfo Vendor="NXP" Name="MIMXRT600_UFL_L0" WorkRAMAddr="0x00000000" WorkRAMSize="0x00480000" Core="JLINK_CORE_CORTEX_M33" JLinkScriptFile="Devices/NXP/iMXRT_UFL/iMXRT6xx_CortexM33.JLinkScript" Aliases="MIMXRT633S; MIMXRT685S_M33"/> <FlashBankInfo Name="Octal Flash" BaseAddr="0x08000000" MaxSize="0x08000000" Loader="Devices/NXP/iMXRT_UFL/MIMXRT_FLEXSPI_UFL_256B_4KB.FLM" LoaderType="FLASH_ALGO_TYPE_OPEN" /> </Device> <!------------------------> <Device> <ChipInfo Vendor="NXP" Name="MIMXRT600_UFL_L1" WorkRAMAddr="0x00000000" WorkRAMSize="0x00480000" Core="JLINK_CORE_CORTEX_M33" JLinkScriptFile="Devices/NXP/iMXRT_UFL/iMXRT6xx_CortexM33.JLinkScript" Aliases="MIMXRT633S; MIMXRT685S_M33"/> <FlashBankInfo Name="Octal Flash" BaseAddr="0x08000000" MaxSize="0x08000000" Loader="Devices/NXP/iMXRT_UFL/MIMXRT_FLEXSPI_UFL_512B_4KB.FLM" LoaderType="FLASH_ALGO_TYPE_OPEN" /> </Device> <!------------------------> <Device> <ChipInfo Vendor="NXP" Name="MIMXRT600_UFL_L2" WorkRAMAddr="0x00000000" WorkRAMSize="0x00480000" Core="JLINK_CORE_CORTEX_M33" JLinkScriptFile="Devices/NXP/iMXRT_UFL/iMXRT6xx_CortexM33.JLinkScript" Aliases="MIMXRT633S; MIMXRT685S_M33"/> <FlashBankInfo Name="Octal Flash" BaseAddr="0x08000000" MaxSize="0x08000000" Loader="Devices/NXP/iMXRT_UFL/MIMXRT_FLEXSPI_UFL_512B_64KB.FLM" LoaderType="FLASH_ALGO_TYPE_OPEN" /> </Device> 2.3 JLINK commander test Please note, the device need to select as MIMXRT600_UFL_L0 when using the QSPI flash. Pic 3                                         pic 4 Pic 5 We can find, the JLINK command can realize the external QSPI flash read, erase function. 2.4 Jflash Test Operation steps: Target->connect->production programming Pic 6 We can find, the Jflash also can realize the RT600 external QSPI flash erase and program. Please note, not all the JLINK can support JFLASH, this document is using Segger JLINK plus. 3 MCUXpresso configuration and test MCUXpresso: v11.4.0 SDK_2_10_0_EVK-MIMXRT685 MCUXPresso IDE import the SDK project, eg. Helloworld or led_output. 3.1 QSPI FCB configuration    FCB is located from the flash offset address 0X08000400, which is used for the FlexSPI Nor boot configuration, the detailed content of the FCB can be found from the RT600 user manual Table 997. FlexSPI flash configuration block. Different external Flash, the configuration is different, if need to use the QSPI flash, the FCB should use the QSPI related configuration and its own LUT table.    Modify SDK project flash_config folder flash_config.c and flash_config.h, LUT contains fast read, status read, write enable, sector erase, block erase, page program, erase the whole chip. If the external QSPI flash command is different, the LUT command should be modified by following the flash datasheet mentioned related command. const flexspi_nor_config_t flexspi_config = { .memConfig = { .tag = FLASH_CONFIG_BLOCK_TAG, .version = FLASH_CONFIG_BLOCK_VERSION, .readSampleClksrc=kFlexSPIReadSampleClk_LoopbackInternally, .csHoldTime = 3, .csSetupTime = 3, .columnAddressWidth = 0, .deviceModeCfgEnable = 0, .deviceModeType = 0, .waitTimeCfgCommands = 0, .deviceModeSeq = {.seqNum = 0, .seqId = 0,}, .deviceModeArg = 0, .configCmdEnable = 0, .configModeType = {0}, .configCmdSeqs = {0}, .configCmdArgs = {0}, .controllerMiscOption = (0), .deviceType = 1, .sflashPadType = kSerialFlash_4Pads, .serialClkFreq = kFlexSpiSerialClk_133MHz, .lutCustomSeqEnable = 0, .sflashA1Size = BOARD_FLASH_SIZE, .sflashA2Size = 0, .sflashB1Size = 0, .sflashB2Size = 0, .csPadSettingOverride = 0, .sclkPadSettingOverride = 0, .dataPadSettingOverride = 0, .dqsPadSettingOverride = 0, .timeoutInMs = 0, .commandInterval = 0, .busyOffset = 0, .busyBitPolarity = 0, .lookupTable = { #if 0 [0] = 0x08180403, [1] = 0x00002404, [4] = 0x24040405, [12] = 0x00000604, [20] = 0x081804D8, [36] = 0x08180402, [37] = 0x00002080, [44] = 0x00000460, #endif // Fast Read [4*0+0] = FLEXSPI_LUT_SEQ(CMD_SDR , FLEXSPI_1PAD, 0xEB, RADDR_SDR, FLEXSPI_4PAD, 0x18), [4*0+1] = FLEXSPI_LUT_SEQ(MODE4_SDR, FLEXSPI_4PAD, 0x00, DUMMY_SDR , FLEXSPI_4PAD, 0x09), [4*0+2] = FLEXSPI_LUT_SEQ(READ_SDR , FLEXSPI_4PAD, 0x04, STOP_EXE , FLEXSPI_1PAD, 0x00), //read status [4*1+0] = FLEXSPI_LUT_SEQ(CMD_SDR , FLEXSPI_1PAD, 0x05, READ_SDR, FLEXSPI_1PAD, 0x04), //write Enable [4*3+0] = FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0x06, STOP_EXE, FLEXSPI_1PAD, 0), // Sector Erase byte LUTs [4*5+0] = FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0x20, RADDR_SDR, FLEXSPI_1PAD, 0x18), // Block Erase 64Kbyte LUTs [4*8+0] = FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0xD8, RADDR_SDR, FLEXSPI_1PAD, 0x18), //Page Program - single mode [4*9+0] = FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0x02, RADDR_SDR, FLEXSPI_1PAD, 0x18), [4*9+1] = FLEXSPI_LUT_SEQ(WRITE_SDR, FLEXSPI_1PAD, 0x04, STOP_EXE, FLEXSPI_1PAD, 0x0), //Erase whole chip [4*11+0]= FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0x60, STOP_EXE, FLEXSPI_1PAD, 0), }, }, .pageSize = 0x100, .sectorSize = 0x1000, .ipcmdSerialClkFreq = 1, .isUniformBlockSize = 0, .blockSize = 0x10000, }; This code has been tested on the RT685+ QSPI flash MT25QL128ABA1ESE, the code boot is working. 3.2 Debug configuration Configure the JLINK options in the MCUXpresso IDE as the JLINK driver: JLinkGDBServerCL.exe Windows->preferences Pic 7 Press debug, generate .launch file. Pic 8 Run->Debug configurations           Pic 9 Choose the device as MIMXRT600_UFL_L0, if the SWD wire is long and not stable, also can define the speed as the fixed low frequency. 3.3 Download and debug test Before download, need to check the RT685 ISP mode configuration, as this document is using the 4 wire QSPI and connect to the FlexSPI A port, so the ISP boot mode should be FlexSPI boot from Port A: ISP2 PIO1_17 low, ISP1 PIO1_16 high, ISP0 PIO1_15 high Click debug button, we can see the code enter the debug mode, and enter the main function, the code address is located in the flexSPI remap address. Pic 10 Click run, we can find the RT685 pin P0_26 is toggling, and the UART interface also can printf information. The application code is working. 4 External SPI flash operation checking To the customer designed board, normally we will use the JLINK command to check whether it can find the ARM core or not at first, make sure the RT chip can work, then will check the external flash operation or not. 4.1 SDK IAP flash code test We can use the SDK related code to test the external flash operation or not at first, the SDK code path is: SDK_2_10_0_EVK-MIMXRT685\boards\evkmimxrt685\driver_examples\iap\iap_flash Then, check the external flash, and modify the code’s related option0, option1 to match the external flash. About the option 0 and option1 definition, we can find it from the RT600 user manual Table 1004.Option0 definition and Table 1005.Option1 definition Pic 11 Pic 12 To the external QSPI flash which is connected to the FLexSPI portA, we can modify the option to the following code:     option.option0.U = 0xC0000001;//EXAMPLE_NOR_FLASH;     option.option1.U = 0x00000000;//EXAMPLE_NOR_FLASH_OPTION1; Then burn the IAP_flash project to the RT685 internal RAM, debug to run it. Pic 13 We can find, the external QSPI flash initialization, erase, read and write all works, and the memory also can find the correct data. 4.2 MCUBootUtility test   Chip enter the ISP mode, then use the MCUBootUtility tool to connect the RT685 and QSPI flash, to do the application code program and read test. ISP mode:ISP2:high, ISP1: high ISP0 low Configure FlexSPI NOR Device Configuration as QSPI, we can use the template: ISSI_IS25LPxxxA_IS25WPxxxA. Pic 14 Click connect to ROM button, check whether it can recognize the external flash: Pic 15 After connection, we can use the tool attached RT685 image to download: NXP-MCUBootUtility-3.3.1\apps\NXP_MIMXRT685-EVK_Rev.E\led_blinky_0x08001000_fdcb.srec Pic 16 We can find, the connection, erase, program and read are all work, it also indicates the RT685+external QSPI flash is working. Then can go to debug it with IDE and debugger.    
View full article
[中文翻译版] 见附件   原文链接: https://community.nxp.com/t5/i-MX-Community-Articles/Effortless-GUI-Development-with-NXP-Microcontrollers/ba-p/1131179  
View full article
                                      配置RT600开发环境 RT600开发入门培训视频。 https://www.nxp.com/document/guide/getting-started-with-i-mx-rt600-evaluation-kit:GS-MIMXRT685-EVK?&tid=vanGS-MIMXRT685-EVK#title2.1   下载I.MX RT600 SDK。下载链接: https://mcuxpresso.nxp.com/en/select?device=EVK-MIMXRT685     下载MCUXpresso IDE。注意需要安装MCUXpresso IDE 11.1.1及最新版本。https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=MCUXPRESSO               下载安装LPCScrypt,可以将默认板载的CMSIS-DAP固件升级改为J-LINK。通过J-LINK,可以下载调试HiFi4 DSP固件。下载链接https://www.nxp.com/design/microcontrollers-developer-resources/lpc-microcontroller-utilities/lpcscrypt-v2-1-1:LPCSCRYPT?&tab=Design_Tools_Tab     下载安装J-LINK驱动。下载链接https://www.segger.com/downloads/jlink/   下载安装Cadence HiFi 4 DSP IDE for MIMXRT600。 第一次下载,注册用户https://tensilicatools.com/register/。国内用户注册时,如果页面没有出现下面人机身份验证,说明IP被GW Firewall屏蔽了。需要通过代理或者其他特殊手段,否则用户注册将无法成功提交。   下载HiFi DSP Development Tools for i.MX RT600开发工具。 https://tensilicatools.com/download/rt600-download-page/   申请License for RT600 SDK。注意输入绑定网卡MAC地址时,需要去除中间‘:’等字符,否则提示失败。   申请成功后,可以下载License文件。   启动Xplorer 8.0.13后,在菜单Help -- Xplorer License Keys安装License文件。安装成功后显示如下:     Xplorer下载调试器配置。 将xt-ocd.exe所在目录加入到系统Path环境变量。   使能”Use XOCD Manager”,指定Topology File   设置Download binary为Always,取消每次下载前都弹出提示框,节省下载时间。     通过J-Link下载HiFi4 DSP固件,可以单步调试代码。    
View full article
The i.MX RT600 crossover MCU combines an ultra-low power MCU with a high performance DSP to enable the next generation of ML/AI, voice and audio applications. Get started today and order your MIMXRT685-EVK.
View full article
i.MX RT6xx The RT6xx is a crossover MCU family is a breakthrough product combining the best of MCU and DSP functionality for ultra-low power secure Machine Learning (ML) / Artificial Intelligence (AI) edge processing, performance-intensive far-field voice and immersive 3D audio playback applications. Fig 1 is the block diagram for the i.MX RT600. It consists of a Cortex-M33 core that runs up to 300 MHz with 32KB FlexSPI cache and an optional HiFi4 DSP that runs up to 600MHz with 96KB DSP cache and 128KB DSP TCM. It also contains a cryptography engine and DSP/Math accelerator in the PowerQuad co-processor. The device has 4.5MB on-chip SRAM. Key features include the rich audio peripherals, the high-speed USB with PHY and the advanced on-chip security. There is a Flexcomm peripheral that supports the configuration of numerous UARTs, SPI, I2C, I2S, etc. Fig 1 Create a eIQ (TensorFlow Lite library) demo In the latest version of SDK for the i.MX RT600, it still doesn't contain the demos about the Machine Learning (ML) / Artificial Intelligence (AI), so it needs the developers to create this kind of demo by themself. To implement it, port the eIQ demos cross from i.MX RT1050/1060 to i.MX RT685 is the quickest way. The below presents the steps of creating a eIQ (TensorFlow Lite library) demo. Greate a new C++ project Install SDK library Fig 2 Create a new C++ project using installed SDK Part In the MCUXpresso IDE User Guide, Chapter 5 Creating New Projects using installed SDK Part Support presents how to create a new project, please refer to it for details Porting tensorflow-lite Copy the tensorflow-lite library to the target project Copy the TensorFlow-lite library corresponding files to the target project Fig 3 Add the paths for the above files Fig 4 Fig 5 Fig 6 Porting main code The main() code is from the post: The “Hello World” of TensorFlow Lite Testing On the MIMXRT685 EVK Board (Fig 7), we record the input data: x_value and the inferenced output data: y_value via the Serial Port (Fig 8). Fig 7 Fig 8 In addition, we use Excel to display the received data against our actual values as the below figure shows. Fig 9 In general, In general, it has replicated the result of the The “Hello World” of TensorFlow Lite Troubleshoot In default, the created project doesn't support print float, so it needs to enable this feature by adding below symbols (Fig 10). Fig 10 When a neural network is executed, the results of one layer are fed into subsequent operations and so must be kept around for some time. The lifetimes of these activation layers vary depending on their position in the graph, and the memory size needed for each is controlled by the shape of the array that a layer writes out. These variations mean that it’s necessary to calculate a plan over time to fit all these temporary buffers into as small an area of memory as possible. Currently, this is done when the model is first loaded by the interpreter, so if the area is not big enough, you’ll see a crash event happen. Regard to this application demo, the default heap size is 4 KB, obviously, it's not big enough to store the model’s input, output, and intermediate tensors, as the codes will be stuck at hard-fault interrupt function (Fig 11). Fig 11 So, how large should we allocate the heap area? That’s a good question. Unfortunately, there’s not a simple answer. Different model architectures have different sizes and numbers of input, output, and intermediate tensors, so it’s difficult to know how much memory we’ll need. The number doesn’t need to be exact—we can reserve more memory than we need—but since microcontrollers have limited RAM, we should keep it as small as possible so there’s space for the rest of our program. We can do this through trial and error. For this application demo, the code works well after increasing ten times than the previous heap size (Fig 12). Fig 12
View full article
This document describes how to use I2S (Inter-IC Sound Bus) and DMA to record and playback audio using NXP's i.MX RT600 crossover MCUs. It also includes the process of how to use the codec chip to process audio data on the i.MX RT600 Evaluation Kit (EVK) based on the Cadence® Tensilica® HiFi4 Audio DSP. Click here to access the full application note.
View full article
Source code: https://github.com/JayHeng/NXP-MCUBootUtility   【v2.0.0】 Features: > 1. Support i.MXRT5xx A0, i.MXRT6xx A0 >    支持i.MXRT5xx A0, i.MXRT6xx A0 > 2. Support i.MXRT1011, i.MXRT117x A0 >    支持i.MXRT1011, i.MXRT117x A0 > 3. [RTyyyy] Support OTFAD encryption secure boot case (SNVS Key, User Key) >     [RTyyyy] 支持基于OTFAD实现的安全加密启动(唯一SNVS key,用户自定义key) > 4. [RTxxx] Support both UART and USB-HID ISP modes >     [RTxxx] 支持UART和USB-HID两种串行编程方式(COM端口/USB设备自动识别) > 5. [RTxxx] Support for converting bare image into bootable image >     [RTxxx] 支持将裸源image文件自动转换成i.MXRT能启动的Bootable image > 6. [RTxxx] Original image can be a bootable image (with FDCB) >     [RTxxx] 用户输入的源程序文件可以包含i.MXRT启动头 (FDCB) > 7. [RTxxx] Support for loading bootable image into FlexSPI/QuadSPI NOR boot device >     [RTxxx] 支持下载Bootable image进主动启动设备 - FlexSPI/QuadSPI NOR接口Flash > 8. [RTxxx] Support development boot case (Unsigned, CRC) >     [RTxxx] 支持用于开发阶段的非安全加密启动(未签名,CRC校验) > 9. Add Execute action support for Flash Programmer >     在通用Flash编程器模式下增加执行(跳转)操作 > 10. [RTyyyy] Can show FlexRAM info in device status >       [RTyyyy] 支持在device status里显示当前FlexRAM配置情况 Improvements: > 1. [RTyyyy] Improve stability of USB connection of i.MXRT105x board >     [RTyyyy] 提高i.MXRT105x目标板USB连接稳定性 > 2. Can write/read RAM via Flash Programmer >    通用Flash编程器里也支持读写RAM > 3. [RTyyyy] Provide Flashloader resident option to adapt to different FlexRAM configurations >     [RTyyyy] 提供Flashloader执行空间选项以适应不同的FlexRAM配置 Bugfixes: > 1. [RTyyyy] Sometimes tool will report error "xx.bat file cannot be found" >     [RTyyyy] 有时候生成证书时会提示bat文件无法找到,导致证书无法生成 > 2. [RTyyyy] Editing mixed eFuse fields is not working as expected >     [RTyyyy] 可视化方式去编辑混合eFuse区域并没有生效 > 3. [RTyyyy] Cannot support 32MB or larger LPSPI NOR/EEPROM device >     [RTyyyy] 无法支持32MB及以上容量的LPSPI NOR/EEPROM设备 > 4. Cannot erase/read the last two pages of boot device via Flash Programmer >    在通用Flash编程器模式下无法擦除/读取外部启动设备的最后两个Page
View full article
The i.MX RT600 MCU includes a Cadence® Tensilica® HiFi 4 DSP running at frequencies of up to 600 MHz.The XOS embedded kernel from Cadence is designed for efficient operation on embedded system built using the Xtensa architecture. Although various parts of XOS continue to be tuned for efficient performance on the Xtensa hardware, most of the code is written in standard C and is not Xtensa-specific. Click here to access the full application note.
View full article
The RT600 is a family of dual-core microcontrollers for embedded applications featuring an Arm® Cortex®-M33 CPU combined with a Cadence® Tensilica ® HiFi 4 audio DSP core.  Check out this latest app note to learn about communication and debugging of these two cores.  For list of all i.MX RT600 app notes, visit: nxp.com/imxrt600
View full article
This document describes how to program a bootable image into the recovery Flash device using i.MX RT600 MCUs. Click here to access the full application note.
View full article
This application note describes how to develop an audio player with NXP i.MX RT600 crossover MCU family. Click here to access the full application note.
View full article