why MfgTool program boot image failure?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

why MfgTool program boot image failure?

3,430 Views
1920844004
Contributor III

 MfgTool  can not display "HID-Compliant vendor-defined device",so failure come.The actual display is shown in the attachment.

anyone who know this? thanks!

0 Kudos
Reply
4 Replies

3,278 Views
jay_heng
NXP Employee
NXP Employee

You can also try this tool, with this tool, You can flash bare image into various boot devices easily and don't need to care about headers (ivt, boot data...)

GitHub - JayHeng/nxp-sec-boot-ui: A one-stop GUI tool to work with NXP MCU (Kinetis, i.MXRT, LPC) RO... 

0 Kudos
Reply

3,278 Views
igorpadykov
NXP Employee
NXP Employee

Hi zhihui

reason may be non-working usb module, one can check usb related

guidelines given in Hardware Development Guide for the MIMXRT1050/MIMXRT1060 Processor
https://www.nxp.com/docs/en/user-guide/MIMXRT105060HDUG.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

3,278 Views
1920844004
Contributor III

I didn't find anything useful. Let me keep going. Thank you.

0 Kudos
Reply

3,278 Views
sicrisreyembay
Contributor II

Check the log file, <Flashloader Location>/Tools/mfgtools-rel/MfgTool.txt

Cause of the failure is indicated in the said log file.

best regards,

Sicris Rey

0 Kudos
Reply