usb vendor specific

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

usb vendor specific

5,170 Views
phuongly1
Contributor I

Hi,

I am trying to implement the usb on imxrt1050 to connect to the vendor server. My usb descriptor is set up as vendor specific class 0xFF, subclass 0x00, protocol 0x00. There is only 1 endpoint1 as Bulk out transfer 0x02 receiver. Currently, I tried to use usb msc example from sdk, I could get the usb connect to the server by correct device descriptor. However, I can not get the data that is sent from the server. Please guide me any example or what do I need to do to get it work. Thank you.

Labels (1)
0 Kudos
Reply
5 Replies

4,932 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Phuong Ly,

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
I'd like to know the more background information, so I was wondering if you introduce what modification you did about the MSC demo which is from the SDK library, in addition, the testing process.
Then I can replicate the phenomenon on my site.
Looking forward to your reply.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

4,932 Views
phuongly1
Contributor I

Hello Jeremy,

Thank you for responding my email. This is the first time I learn and work on USB. There is a lot of things that I have no clue ☹. Here is this my configuration descriptor that I need to config. I need to receive the big data is send from the vendor server to usb

USB_DMA_INIT_DATA_ALIGN(USB_DATA_ALIGN_SIZE)

uint8_t g_UsbDeviceConfigurationDescriptor[] = {

9U, // bLength;

2U, // bDescriptorType;

USB_SHORT_GET_LOW(99799), // wTotalLength

USB_SHORT_GET_HIGH(99799),

2U, // bNumInterfaces

1U, // bConfigurationValue

0U, // iConfiguration

0x80U, // bmAttributes

50U, // bMaxPower

// interface descriptor, USB spec 9.6.5, page 267-269, Table 9-12

9U, // bLength

4U, // bDescriptorType

0U, // bInterfaceNumber

0U, // bAlternateSetting

1U, // bNumEndpoints

0xffU, // bInterfaceClass (Vendor specific)

0x00U, // bInterfaceSubClass

0x00U, // bInterfaceProtocol

0U, // iInterface

// endpoint descriptor, USB spec 9.6.6, page 269-271, Table 9-13

7U, // bLength

5U, // bDescriptorType

1U, // bEndpointAddress

0x02U, // bmAttributes (0x02=bulk)

64U, 0U, // wMaxPacketSize

0U, // bInterval

// interface descriptor, DFU Mode (DFU spec Table 4.4)

9U, // bLength

4U, // bDescriptorType

1U, // bInterfaceNumber

0U, // bAlternateSetting

0U, // bNumEndpoints

0xFEU, // bInterfaceClass

0x01U, // bInterfaceSubClass

0x01U, // bInterfaceProtocol (Runtime)

4U, // iInterface

// DFU Functional Descriptor (DFU spec TAble 4.2)

9U, // bLength

0x21U, // bDescriptorType

0x0DU, // bmAttributes

USB_SHORT_GET_LOW(DFU_DETACH_TIMEOUT), // wDetachTimeOut

USB_SHORT_GET_HIGH(DFU_DETACH_TIMEOUT),

USB_SHORT_GET_LOW(DFU_TRANSFER_SIZE), // wTransferSize

USB_SHORT_GET_HIGH(DFU_TRANSFER_SIZE),

0x01,0x01, // bcdDFUVersion

};

I am using sdk of usb mcs lite example code. I removed some of Buld in and UFI configuration because I won’t need them. Right now I could connect my usb to the vendor server by correct device descriptor but that is it. When the server send data my usb response with broken pipe as picture (Data on the left is my working usb with broken pipe. Data on the right is support to be from vendor device).

  • In function USB_DeviceMscBulkOut(),my usb is always break in else case with

mscHandle->outEndpointStallFlag = 1;

mscHandle->inEndpointStallFlag = 1;

mscHandle->stallStatus = (uint8_t)USB_DEVICE_MSC_STALL_IN_CBW;

mscHandle->performResetRecover = 1;

So I tried to change these flags to 0 to make the usb is not in stall state. Please guide me how to set up this BullkOut function (which flags should I need to remove or keep)

  • I don’t understand how does the interrupt void USB_OTG1_IRQHandler(void) work?. For my code, it only trigger when those descriptors are setting up, but after that it is not at all.

  • Should I use the function USB_DeviceMscRecv() for receiving data ? what should I modify it?

  • Do I need to do any thing about pipe?

Thank you very much for trouble

Phuong

0 Kudos
Reply

4,932 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Phuong Ly,

Thanks for your reply.
It makes me a bit confused, according to your statement, you just said you want to receive big data from the host.
However, you have not clarified what USB class device you want to implement, in further, I was wondering if you can introduce what modification you did about the MCS lite example code.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

4,932 Views
phuongly1
Contributor I

Hi Jeremy,

I actually did send you some modification on the last email.

I want to receive big data that is sent from the host. I want to implement usb vendor class 0xFF that has only one endpoint 1 as BULK_OUT. I only get the device control config on endpoint0 then I stuck. In the attachment file (captured by wireshark), the last BULK OUT response from usb is error when the host sends big data (1600 bytes). Then interrupt is stopped triggering after that. Here is my modified code and descriptors

USB_DMA_INIT_DATA_ALIGN(USB_DATA_ALIGN_SIZE)

uint8_t g_UsbDeviceDescriptor[] = {

USB_DESCRIPTOR_LENGTH_DEVICE, /* Size of this descriptor in bytes */

USB_DESCRIPTOR_TYPE_DEVICE, /* DEVICE Descriptor Type */

USB_SHORT_GET_LOW(USB_DEVICE_SPECIFIC_BCD_VERSION),

USB_SHORT_GET_HIGH(USB_DEVICE_SPECIFIC_BCD_VERSION), /* USB Specification Release Number in

Binary-Coded Decimal (i.e., 2.10 is 210H). */

USB_DEVICE_CLASS, /* Class code 0x00 */

USB_DEVICE_SUBCLASS, /* Subclass code 0x00 */

USB_DEVICE_PROTOCOL, /* Protocol code 0x00 */

USB_CONTROL_MAX_PACKET_SIZE, /* Maximum packet size for endpoint zero is 64*/

USB_SHORT_GET_LOW(VENDOR_ID), USB_SHORT_GET_HIGH(VENDOR_ID), /* Vendor ID (assigned by the USB-IF) */

USB_SHORT_GET_LOW(PRODUCT_ID), USB_SHORT_GET_HIGH(PRODUCT_ID), /* Product ID (assigned by the manufacturer) */

USB_SHORT_GET_LOW(DEVICE_VER), USB_SHORT_GET_HIGH(DEVICE_VER), /* Device release number in binary-coded decimal */

0x01U, /* Index of string descriptor describing manufacturer */

0x02U, /* Index of string descriptor describing product */

0x03U, /* Index of string descriptor describing the device's serial number */

USB_CONFIGURE_COUNT, /* Number of possible configurations is 1 */

};

USB_DMA_INIT_DATA_ALIGN(USB_DATA_ALIGN_SIZE)

uint8_t g_UsbDeviceConfigurationDescriptor[] = {

USB_DESCRIPTOR_LENGTH_CONFIGURE, /* Size of this descriptor in bytes 0x09*/

USB_DESCRIPTOR_TYPE_CONFIGURE, /* CONFIGURATION Descriptor Type 0x02*/

USB_SHORT_GET_LOW(CONFIG_DESC_SIZE ), /* CONFIG_DESC_SIZE 9 + 9 + 7 + 9 + 9*/

USB_SHORT_GET_HIGH(CONFIG_DESC_SIZE), /* Total length of data returned for this configuration. */

USB_MSC_INTERFACE_COUNT, /* Number of interfaces supported by this configuration is 2*/

USB_MSC_CONFIGURE_INDEX, /* Value to use as an argument to the SetConfiguration() request to select this configuration is 1*/

0U, /* Index of string descriptor describing this configuration */

(USB_DESCRIPTOR_CONFIGURE_ATTRIBUTE_D7_MASK) |

(USB_DEVICE_CONFIG_SELF_POWER << USB_DESCRIPTOR_CONFIGURE_ATTRIBUTE_SELF_POWERED_SHIFT) |

(USB_DEVICE_CONFIG_REMOTE_WAKEUP << USB_DESCRIPTOR_CONFIGURE_ATTRIBUTE_REMOTE_WAKEUP_SHIFT),

/* Configuration characteristics

D7: Reserved (set to one)

D6: Self-powered

D5: Remote Wakeup

D4...0: Reserved (reset to zero)

*/

USB_DEVICE_MAX_POWER, /* Maximum power consumption of the USB

  • device from the bus in this specific

  • configuration when the device is fully

  • operational. Expressed in 2 mA units

  • (i.e., 50 = 100 mA).

*/

USB_DESCRIPTOR_LENGTH_INTERFACE, /* Size of this descriptor in bytes 0x09 */

USB_DESCRIPTOR_TYPE_INTERFACE, /* INTERFACE Descriptor Type 0x04*/

USB_MSC_INTERFACE_INDEX, /* Number of this interface 0x00 */

0x00U, /* Value used to select this alternate setting

for the interface identified in the prior field */

USB_MSC_ENDPOINT_COUNT, /* Number of endpoints used by this interface (excluding endpoint zero) is 0x01 */

VENDOR_SPEC_CLASS, /* Class code 0xFF */

0, /* Subclass code (assigned by the USB-IF). */

0, /* Protocol code (assigned by the USB). */

0x00U, /* Index of string descriptor describing this interface */

USB_DESCRIPTOR_LENGTH_ENDPOINT, /* Size of this descriptor in bytes 0x07 */

USB_DESCRIPTOR_TYPE_ENDPOINT, /* ENDPOINT Descriptor Type 0x01 */

USB_MSC_BULK_OUT_ENDPOINT| (USB_OUT << USB_DESCRIPTOR_ENDPOINT_ADDRESS_DIRECTION_SHIFT), /* The address of the endpoint on the USB device

//described by this descriptor. */

USB_ENDPOINT_BULK, /* This field describes the endpoint's attributes */

USB_SHORT_GET_LOW(FS_MSC_BULK_OUT_PACKET_SIZE), /*size is 64 */

USB_SHORT_GET_HIGH(FS_MSC_BULK_OUT_PACKET_SIZE),

0x00U, /Useless for bulk in endpoint/

// interface descriptor, DFU Mode (DFU spec Table 4.4)

9, // bLength

4, // bDescriptorType

DFU_INTERFACE, // bInterfaceNumber

0, // bAlternateSetting

0, // bNumEndpoints

0xFE, // bInterfaceClass

0x01, // bInterfaceSubClass

0x01, // bInterfaceProtocol (Runtime)

4, // iInterface

// DFU Functional Descriptor (DFU spec TAble 4.2)

9, // bLength

0x21, // bDescriptorType

0x0D, // bmAttributes

USB_SHORT_GET_LOW(DFU_DETACH_TIMEOUT), // wDetachTimeOut

USB_SHORT_GET_HIGH(DFU_DETACH_TIMEOUT),

USB_SHORT_GET_LOW(DFU_TRANSFER_SIZE), // wTransferSize

USB_SHORT_GET_HIGH(DFU_TRANSFER_SIZE),

0x01,0x01, // bcdDFUVersion

};

In function USB_DeviceMscBulkOut(), comment

if (!mscHandle->transferRemaining)

{

mscHandle->dataOutFlag = 0;

{

// USB_DeviceSendRequest(g_msc.deviceHandle, mscHandle->bulkInEndpoint, (uint8_t *)mscHandle->mscCsw,

// USB_DEVICE_MSC_CSW_LENGTH);

//increase the size USB_DEVICE_MSC_CSW_LENGTH from 31 to 64

USB_DeviceSendRequest(g_msc.deviceHandle, mscHandle->bulkInEndpoint, (uint8_t *)mscHandle->mscCsw,

64);

mscHandle->cswPrimeFlag = 1;

}

}

// else if ((mscHandle->cbwValidFlag) && (event->length == USB_DEVICE_MSC_CBW_LENGTH) &&

// (mscHandle->mscCbw->signature == USB_DEVICE_MSC_DCBWSIGNATURE) &&

// (!((mscHandle->mscCbw->logicalUnitNumber & 0xF0) || (mscHandle->mscCbw->cbLength & 0xE0))) &&

// (mscHandle->mscCbw->logicalUnitNumber < (mscHandle->logicalUnitNumber + 1)) &&

// ((mscHandle->mscCbw->cbLength >= 0x01) && (mscHandle->mscCbw->cbLength <= 0x10)))

// {

//put the code below instead.

else if ((mscHandle->cbwValidFlag) && (event->length == 64))

{

……

}

//comment out error = USB_DeviceMscProcessUfiCommand(mscHandle); //make it return success

//comment out

// if (!((mscHandle->dataOutFlag) || ((mscHandle->dataInFlag) || (mscHandle->needInStallFlag))))

// {

// USB_DeviceSendRequest(g_msc.deviceHandle, mscHandle->bulkInEndpoint, (uint8_t *)mscHandle->mscCsw,

// USB_DEVICE_MSC_CSW_LENGTH);

// mscHandle->cswPrimeFlag = 1;

// }

  • In function USB_DeviceMscEndpointsInit(), comment out

// epCallback.callbackFn = USB_DeviceMscBulkIn; //phuong

// epCallback.callbackParam = (void *)&g_msc.mscStruct;

//

// epInitStruct.zlt = 0;

// epInitStruct.transferType = USB_ENDPOINT_BULK;

// epInitStruct.endpointAddress =

// USB_MSC_BULK_IN_ENDPOINT | (USB_IN << USB_DESCRIPTOR_ENDPOINT_ADDRESS_DIRECTION_SHIFT);

// g_mscHandle->bulkInEndpoint = epInitStruct.endpointAddress;

// if (USB_SPEED_HIGH == g_msc.speed)

// {

// epInitStruct.maxPacketSize = HS_MSC_BULK_IN_PACKET_SIZE;

// }

// else

// {

// epInitStruct.maxPacketSize = FS_MSC_BULK_IN_PACKET_SIZE;

// }

//

// USB_DeviceInitEndpoint(g_msc.deviceHandle, &epInitStruct, &epCallback);

  • In function USB_DeviceCallback()

case kUSB_DeviceEventSetConfiguration:

if (g_mscHandle->configuration == *temp8)

{

break;

}

if (g_mscHandle->configuration)

{

USB_DeviceMscEndpointsDeinit();

}

g_mscHandle->configuration = *temp8;

if (USB_MSC_CONFIGURE_INDEX == (*temp8))

{

/USB_DeviceMscEndpointsDeinit();/

error = USB_DeviceMscEndpointsInit();

// USB_DeviceRecvRequest(g_msc.deviceHandle, g_mscHandle->bulkOutEndpoint, (uint8_t *)g_mscHandle->mscCbw,

// USB_DEVICE_MSC_CBW_LENGTH);

USB_DeviceRecvRequest(g_msc.deviceHandle, g_mscHandle->bulkOutEndpoint, (uint8_t *)g_mscHandle->mscCbw,

64); //phuong

g_mscHandle->cbwPrimeFlag = 1;

g_msc.attach = 1;

}

break;

  • In function USB_DeviceApplicationInit()

// ufi->requestSense = &g_requestSense;

// ufi->readCapacity = &g_readCapacity;

// ufi->readCapacity16 = &g_readCapacity16;

// ufi->formatCapacityData = &g_formatCapacityData[0];

//

// ufi->requestSense->validErrorCode = USB_DEVICE_MSC_UFI_REQ_SENSE_VALID_ERROR_CODE;

// ufi->requestSense->additionalSenseLength = USB_DEVICE_MSC_UFI_REQ_SENSE_ADDITIONAL_SENSE_LEN;

// ufi->requestSense->senseKey = USB_DEVICE_MSC_UFI_NO_SENSE;

// ufi->requestSense->additionalSenseCode = USusbB_DEVICE_MSC_UFI_NO_SENSE;

// ufi->requestSense->additionalSenseQualifer = USB_DEVICE_MSC_UFI_NO_SENSE;

//

// ufi->readCapacity->lastLogicalBlockAddress = USB_LONG_TO_BIG_ENDIAN(g_mscHandle->totalLogicalBlockNumber - 1);

// ufi->readCapacity->blockSize = USB_LONG_TO_BIG_ENDIAN((uint32_t)g_mscHandle->lengthOfEachLba);

// ufi->readCapacity16->lastLogicalBlockAddress1 = USB_LONG_TO_BIG_ENDIAN(g_mscHandle->totalLogicalBlockNumber - 1);

// ufi->readCapacity16->blockSize = USB_LONG_TO_BIG_ENDIAN((uint32_t)g_mscHandle->lengthOfEachLba);

// by phuong

I know there is a lot of flag of mscHandle that I don’t need that should be removed. However, there were so many of them tangle together that I don’t understand clearly their purpose. Please give me suggestion.

Thank you very much

Phuong

0 Kudos
Reply

4,932 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Phuong Ly,

Thanks for your reply.
According to your reply, I guess you would like to create a DFU class device base on MSC demo, however, it doesn't well, is it right?
In further, after a review of attachment, I don't find the process of enumeration, I was wondering if you can share it.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply