Hello,
i want to work with the ADC on the RT1050. Therefor i imported the example "evkbimxrt1050_adc_12b1msps_sar_interrupt". I routed the ADC IN0 to the connectors J13.
The first question:
As J13 is a 2x Pin header, which header is used?
I connected a variable voltage source with + to J13 Pin1 and - to TB1 for grounding.
The debuging process usw works fine and everytime i press a keyboard button the program returns a value. The main problem is that the returning value is almost constant. It doesnt matter if i power the adc input with 0.1V or 1.0V.
Have i forgot some config settings?
best regards,
Andy