pwm.h file not available for LED dimming

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

pwm.h file not available for LED dimming

1,365 次查看
cgupta
Contributor I
Hi I am trying to use LED dimming function of LED software component but cannot as pwm component required for the same is not available in any of the SDk's. I am working with i.MX RT 1062. Let me know if I can download it from a different source. Regards Chinmay
0 项奖励
回复
3 回复数

1,363 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
Whether you want to download a particualr LED dimming function library.
However, the PWM implementation in SDK library doesn't meet your requirement.
Is my understanding right?
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复

1,361 次查看
cgupta
Contributor I

Hi Jeremy,

LED_Dimming is given as a #define in LED.c, when I enable that it tries to include pwm.h(as per SDK 2.8.6) or fsl_adapter_pwm.h(as per 2.9.2) but these files are not there in both the SDK's. 

I require fsl_adapter_pwm.h to make LED dimming effect work.

 

Regards
Chinmay 

0 项奖励
回复

1,349 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi,
After checking, the led software component hasn't been ready until now.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复