microSD card data line pull-up resistor in RT1052

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

microSD card data line pull-up resistor in RT1052

Jump to solution
1,180 Views
deega_jung
Contributor III

Hello NXP community,

Inquiry of the microSD card data line pull-up resistor,

According to AN10911, MicroSD CARD's DAT0/1/2 line has recommended the pull-up resistor. However, the EV-Kit reference circuit of RT105x uses only DAT0 pull-up, and DAT1/2 does not have pull-up.

What's the reason?

 

Thanks,

Deega

Labels (1)
0 Kudos
Reply
1 Solution
1,171 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) What's the reason?
-- The alternative method is to enable the internal pull-up resistor, in another word, the external resistor is not definitely necessary.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

2 Replies
1,172 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) What's the reason?
-- The alternative method is to enable the internal pull-up resistor, in another word, the external resistor is not definitely necessary.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

1,155 Views
deega_jung
Contributor III

Hi TIC,

Thank you for your comments.

 

Thanks,

Deega

0 Kudos
Reply