issues with configuring spread spectrum on the RT1170.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

issues with configuring spread spectrum on the RT1170.

跳至解决方案
1,387 次查看
sajithdevidas
Contributor III
Hi,
We are working with custom boards based on the RT1170, and using the MCU Xpresso IDE. To pass the EMI/EMC test, we need to drive the SEMC clock root through any of the main clocks that support spread spectrum. However, according to the datasheet, SEMC only supports the following main clocks which is having spread spectrum
 
- SEMC_ClockRoot_MuxSysPll1Div5
- SEMC_ClockRoot_MuxSysPll2Out
- SEMC_ClockRoot_MuxSysPll2Pfd1
 
Except for these clocks, all the others do not support spread spectrum. We attempted to work with PLL2, but encountered the following error
sajithdevidas_0-1709304729735.png

 

 I am providing a forum link that discusses a similar issue.
sajithdevidas_1-1709304730150.png

 

Trying to enable SSC on RT1170 EVK with MCUXpresso. Ref: AN12879 Steps: 1. Base project: SDK Example evkmimxrt1170_semc_cm7 2. Using IDE to config SSC  3. Boot failed 4. Sometimes can boot normally (~ 1/50) Any step I missed? Regards Seen
community.nxp.com
 
 
The alternative option is to drive it through PLL1. According to AN12879, for instance, we are attempting to set 12MHz as the range and 60Hz as the step. However, configuring this through the configtools has not been successful. There are various constraints to consider, such as the input being 24MHz, the output being 1GHz, etc. Also, setting the range and step has been unsuccessful.
sajithdevidas_2-1709304729741.png

 

 
Kindly address this issue and provide a reply as soon as possible. Thank you.
 
Sajith P
0 项奖励
回复
1 解答
1,310 次查看
sajithdevidas
Contributor III

 

Hi @Kan_Li 

We have identified the issue. The code includes lvgl, and in the linker script, we are including "bss.ldt", which is taking up extra space.

<#if memory.name=="SRAM_OC1"> *(.bss*) </#if>
 

After removing the "bss.ldt" file, the spread spectrum feature is enabled successfully.

However, a new issue has arisen. The boot-up time of my code has increased to 2-3 seconds, whereas previously it was instantaneous. This delay occurs only when spread spectrum is enabled. If I disable spread spectrum, the boot-up time returns to normal.

Please respond as soon as possible. Thank you for your patience

 

在原帖中查看解决方案

0 项奖励
回复
7 回复数
1,347 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @sajithdevidas ,

 

Did you try the demo from https://community.nxp.com/t5/i-MX-RT/i-MX-RT1170-Failed-to-boot-after-Spread-Spectrum-Clocking-is/m-... on RT1170 EVK? Does it work or still fail? Please kindly clarify.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

0 项奖励
回复
1,345 次查看
sajithdevidas
Contributor III

Yes, i tried,
But my code is working on SDRAM, and when i am trying to put the fsl_clock.c into the SRAM_OC1, but the fsl_clock.o is of 3.3MB, i don't know why it is this much big, and it is not fit in that region,

sajithdevidas_0-1709537380859.png

 

 

标记 (1)
0 项奖励
回复
1,320 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @sajithdevidas ,

 

The demo would not take so many memory resource, did you change it according to your custom board? It just takes about 10k here for SRAM_OC1.

Kan_Li_0-1709542477831.png

 

Is it possible to share your code for a review?

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

0 项奖励
回复
1,311 次查看
sajithdevidas
Contributor III

 

Hi @Kan_Li 

We have identified the issue. The code includes lvgl, and in the linker script, we are including "bss.ldt", which is taking up extra space.

<#if memory.name=="SRAM_OC1"> *(.bss*) </#if>
 

After removing the "bss.ldt" file, the spread spectrum feature is enabled successfully.

However, a new issue has arisen. The boot-up time of my code has increased to 2-3 seconds, whereas previously it was instantaneous. This delay occurs only when spread spectrum is enabled. If I disable spread spectrum, the boot-up time returns to normal.

Please respond as soon as possible. Thank you for your patience

 

0 项奖励
回复
1,291 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @sajithdevidas ,

 

It is hard to advise without your code, so is it possible to tell us how you disable spread spectrum and how you enable it? Thanks for your patience!

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

0 项奖励
回复
1,265 次查看
sajithdevidas
Contributor III

thank you @Kan_Li ,
the issue has been solved,

0 项奖励
回复
1,331 次查看
sajithdevidas
Contributor III

hi @Kan_Li ,

we are not using RT1170 EVK board, we are using our own custom board which runs on RT1176xx

 

标记 (1)
0 项奖励
回复