imxrt1052 flex io i2c dma

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

imxrt1052 flex io i2c dma

跳至解决方案
1,346 次查看
ccc_clive
Contributor III

flexio I2C 支持dma吗,我看其他的 spi uart I2S 都支持dma(sdk包里面有相关库文件),但是I2C dma的库文件就没有

标签 (1)
0 项奖励
回复
1 解答
1,304 次查看
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello
I hope you are well.

FlexIO supports DMA, if FlexIO is configured as I2C however there are no specifical drivers for this. You need to refer to the already existing FlexIO uart/spi/… to implement one for i2c.

Best regards,
Omar

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,305 次查看
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello
I hope you are well.

FlexIO supports DMA, if FlexIO is configured as I2C however there are no specifical drivers for this. You need to refer to the already existing FlexIO uart/spi/… to implement one for i2c.

Best regards,
Omar

0 项奖励
回复