imxrt1052 flex io i2c dma

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imxrt1052 flex io i2c dma

Jump to solution
1,285 Views
ccc_clive
Contributor III

flexio I2C 支持dma吗,我看其他的 spi uart I2S 都支持dma(sdk包里面有相关库文件),但是I2C dma的库文件就没有

Labels (1)
0 Kudos
Reply
1 Solution
1,243 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello
I hope you are well.

FlexIO supports DMA, if FlexIO is configured as I2C however there are no specifical drivers for this. You need to refer to the already existing FlexIO uart/spi/… to implement one for i2c.

Best regards,
Omar

View solution in original post

0 Kudos
Reply
1 Reply
1,244 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello
I hope you are well.

FlexIO supports DMA, if FlexIO is configured as I2C however there are no specifical drivers for this. You need to refer to the already existing FlexIO uart/spi/… to implement one for i2c.

Best regards,
Omar

0 Kudos
Reply