imxrt1052 emwin with pxp

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imxrt1052 emwin with pxp

312 Views
ccc_clive
Contributor III

I have find the pxp drive in emwin 6.32.But i test it with lcd formart rgb565, it not work well with 32bit memory device. The scene is that, i draw a png picture with rotation fucntion(any angle),so i use 32bit memory device to rotate it, it not work well and it make lcd frame buff into exception that point(0,0) position changed. i guess it is draw 32bit memory to lcd frame buff.  without this(32bit memory device ),it is work well. is it only for argb8888? 

0 Kudos
Reply
1 Reply

264 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @ccc_clive,

Please refer to my response on the following community post for more information about how to adequately integrate PXP with emWin: emWin: Adding PXP to LCD_X_Config() - NXP Community.

BR,
Edwin.

0 Kudos
Reply