imxrt LQFP SDRAM reliability

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imxrt LQFP SDRAM reliability

Jump to solution
3,398 Views
martinribelotta
Contributor I

My design use a imxrt1021 in LQFP144 package and a 32MB SDRAM directly connected routed in 2-layer board with good GND plane but with great distance for the plane (due to tickness of 2-layer PCB). This produce impedance mismatch for DQn/Dn/CKx/etc.

The design files is in:

GitHub - martinribelotta/imxrt1020-module: iMX RT 1020 CPU module 

In the hardware design manual it advice to put resistors on the pins of data and directions to avoid the reflection of the signals due to impedance mismatching. The dimensions of recommended tracks/vias in the PCB design rules is apparently specified for a 4-layer PCB with standard stackup, not for 2-layer.

But... when I see the refernece design (MIMXRT1020-EVK design files) the series resistors is 0ohm (sheet 12 of the document "SPF-29856_A3.pdf" inner MIMXRT1020-EVK-Design-Files.zip file)

pastedImage_1.png

The gerbers in the design package show a bad GND plane and many lines crossing. This is good practice? 

Viewing this question:

Is the SDRAM on the 1020 EVK broken? 

I have the following doubts:

  • Is reliable the routing of 1020 EVK?
  • The R0 ohm in serie with data/address/control/clock lines is necesary?
  • The absence of good ground plane is problematic?
  • In any case... The problems may mitigate dropping down the CLK frecuency of SDRAM?

Many thanks for the time.

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
2,948 Views
igorpadykov
NXP Employee
NXP Employee

> DSR level 3 strength on the SDRAM drivers. I not localize any reference in RefMan:

drive strength is configured by DSE field of IOMUXC_SW_PAD_CTL_PAD.. register,

for example sect.34.7.171 SW_PAD_CTL_PAD_GPIO_AD_B0_04 SW PAD Control
Register (IOMUXC_SW_PAD_CTL_PAD_GPIO_AD_B0_04) i.MX RT1050 Processor Reference Manual
https://www.nxp.com/docs/en/reference-manual/IMXRT1050RM.pdf

Best regards
igor

View solution in original post

0 Kudos
Reply
4 Replies
2,948 Views
igorpadykov
NXP Employee
NXP Employee

Hi Martin

recommended to follow guidelines provided in

Hardware Development Guide for the MIMXRT1050/MIMXRT1060 Processor 
https://www.nxp.com/docs/en/user-guide/MIMXRT105060HDUG.pdf

Reference board was designed when not all documentation was prepared so

it may differ from recommendations in Hardware Development Guide.

> problems may mitigate dropping down the CLK frecuency of SDRAM?

yes

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
2,948 Views
martinribelotta
Contributor I

Maybe you refer of this:

https://www.nxp.com/docs/en/nxp/user-guides/MIMXRT1020HDUG.pdf 

For mimxrt1020 two layer board route? (section 8: Two (p)layer board design)

Ideally, all this problems have solution in a 4layer standard PCB with basic high speed stackup but the cost increase and the imxrt102x family is designed for low cost design (for a 4 layer board is preferable the imxrt1050/60)

In the section 7.1 (stackup) I cannot calculate the same impedance than the document with standard FR4:

pastedImage_2.png

The trace impedance with this dimensions and 56mils of stackup space is 150 ohm in standard FR4 with ER 4.3 if my calculus is right.

I accomplished with all rules in section 7.5 of the same document.

In section 8.4 this recommend said:

Also, it’s found that it needs to lower to SDRAM drive strength to DSR level 3 in software to balance 133MHz R/W speed and board EMC performance.

This paragraph reference to DSR level 3 strength on the SDRAM drivers. I not localize any reference in RefMan:

https://www.nxp.com/docs/en/reference-manual/IMXRT1020RM.pdf 

Of this register. Some additional info?

Again, many thanks for your time.

0 Kudos
Reply
2,949 Views
igorpadykov
NXP Employee
NXP Employee

> DSR level 3 strength on the SDRAM drivers. I not localize any reference in RefMan:

drive strength is configured by DSE field of IOMUXC_SW_PAD_CTL_PAD.. register,

for example sect.34.7.171 SW_PAD_CTL_PAD_GPIO_AD_B0_04 SW PAD Control
Register (IOMUXC_SW_PAD_CTL_PAD_GPIO_AD_B0_04) i.MX RT1050 Processor Reference Manual
https://www.nxp.com/docs/en/reference-manual/IMXRT1050RM.pdf

Best regards
igor

0 Kudos
Reply
2,948 Views
martinribelotta
Contributor I

Perfect. I found the rigth way to match impedances on my design.

pastedImage_1.png

(from IMXRT1020RM.pdf)

0 Kudos
Reply