Hi,
We would like to set the eFUSE for booting from a QSPI NOR Flash without depending on the BOOT pins as struggling with IOs availability for a custom board. Could you please guide me how to burn these eFUSE on the chip using MCUXpresso IDE? We have a JTAG connection for programming and debugging! Serial/USB to serial connection is available to connect to a PC for debugging purpose. I am not sure if we can attach a tool to it for setting this fuse.
Thanks & regards,
Rajani
Hello Rajani,
Hope you are doing well.
There are several tools that can help you burn the fuses. I'll list them here:
1. MCUBootUtility Tool:
- Please keep in mind that to burn the fuses using this utility you need to use either USB or UART while the RT is in serial downloader mode
2. MCUXpresso Secure Provisioning Tool:
- Direct connection to the target via UART, USB-HID for provisioning and programming
3. It is also possible to burn the fuses in runtime, please refer to the following thread:
How to burn BT_FUSE_SEL on RT1050.
Best Regards,
Sabina
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Stefan,
Thank you for your advice.
I was hoping to use MCUBootUtility or MCU Secure Provisioning Tool through a JTAG connection to both burn fuses and program firmware, instead of USB or UART. A small JTAG footprint seems to be more acceptable to our designers than a USB connector or a UART pin header.
I was trying to keep production steps simple and to not write a dedicated piece of software for production but it seems to be the way to go if that is not supported by any NXP tool.
Best regards,
Raul Tierno