Hello,
There is the same question with the case. So I will handle your question for the case. Please check your email in time.
Have a nice day.
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------
hello,
I confirm I can't find the COM port when I run the board , but meanwhile I canUse JFLASH to connect to the corresponding development board and burn.
I tried ,but failed.
hello,this can't miss this COM drive problem,because I can find the COM port when i run the 1050 development borad .