image_enc2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,426件の閲覧回数
dark0711
Contributor III

I’m trying to set up a RT1064 board to boot using BEE SW-GP2 keys as in the https://community.nxp.com/t5/i-MX-RT-Knowledge-Base/RT1015-APP-BEE-encryption-operation-method/ta-p/... but cannot download the image_enc2.zip file from the Chinese link https://www.cnblogs.com/henjay724/p/10189602.html . Is could I get this file another way?

0 件の賞賛
返信
1 解決策
2,414件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
To provide the fastest possible support, I've attached the image_enc2.zip file, please check it.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,409件の閲覧回数
dark0711
Contributor III

Thanks for the help

 
0 件の賞賛
返信
2,415件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
To provide the fastest possible support, I've attached the image_enc2.zip file, please check it.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信