iMXRT1010 svd file

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMXRT1010 svd file

2,037 Views
gfisys
Contributor I

Anyone knows where I can get the SVD file for the iMXRT1010 chip?

0 Kudos
Reply
6 Replies

1,993 Views
Masmiseim
Senior Contributor I
0 Kudos
Reply

1,987 Views
gfisys
Contributor I

Thanks so much! I appreciate it.

0 Kudos
Reply

2,026 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @gfisys ,

You can extract the CMSIS-SVD files from the NXP MCUXpresso SDK: they are just using an .xml extension instead of the standard .svd one.

 

Regards,

Jing

0 Kudos
Reply

2,023 Views
gfisys
Contributor I

Thanks for the tip @jingpan 

 

I searched the SDK folder and subfolders, but the only xml file that looks like an svd file is this one: 'MIMXRT1011xxxxx_manifest_v3_10.xml'. I tried to load this file into my Segger embedded studio IDE, but it doesn't seem to recognize it as a proper SVD file. Is that the correct file?

 

 

0 Kudos
Reply

1,976 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @gfisys ,

You can find it in SDK_2_13_0_MIMXRT1020-EVK\devices\MIMXRT1020.

 

Regards,

Jing

0 Kudos
Reply

2,004 Views
gfisys
Contributor I

@jingpan can you tell me the exact location inside the MCUExpresso SDK where the xml file you mentioned resides? Cause I can't find the file. Or, if you have the file can you send it to me? Thanks.

 

 

0 Kudos
Reply