Hi Udo Eberhardt,
Today I check your question with our hardware engineer, why the R169 is not connected.
This resistor is not connect, just make sure the hyper flash reset is not reset when the RT chip want to read the code from external hyper flash. As you know, if the code put in the hyper flash, after RT POR, the chip will run from the external hyper flash, if something else control the hyper flash reset pin to low, it will cause the code read failed.
So, to keep safe, the hyper flash reset pin just add the pull up resistor, it will reset after flash chip POR. I don't know why you need the external flash be reset when the RT reset at the same time? You just need to make the external hyper flash works when the RT want to read it, even the RT do other reset, you don't need to reset the external flash chip.
But if you want to reset at the same time, I have been told, when use internal software reset SYSRESETREQ, the RT POR pin will also be reset, so you can connect the external flash reset pin to POR pin.
If you want to control the external flash reset freely, you also can use the RT GPIO pin to control it, you can find a GPIO as input pin, and in the hyper flash reset pin add an external 10k pull up resistor.
Wish it helps you!
Have a great day,
Kerry
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------