iMX RT1170 Shared Memory

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX RT1170 Shared Memory

1,655 Views
BTasdemir
Contributor I

Hi,

I split the OCRAM area. Im using 0x20338000 address for sharing datas. I write data from M4 core to this address and then I want to read same datas in same address. When I read from M4, I can see that the data has changed but when I read from M7, I cannot see that the data has changed. If I stop the code with a breakpoint, the data is updated.

0 Kudos
Reply
3 Replies

1,641 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @BTasdemir ,

I think it's most probably caused by cache. OCRAM is cacheable.  And both M7 and M4 core has cache.

 

Regards,

Jing

0 Kudos
Reply

1,632 Views
BTasdemir
Contributor I

Hi @jingpan

Which ram region should I use for this ?

0 Kudos
Reply

1,585 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @BTasdemir ,

You can set the area to noncacheable. Please refer to the function BOARD_ConfigMPU().

 

Regards,

Jing

0 Kudos
Reply