iMX RT1020 Reference Manual - SRK_REVOKE missing from fusemap?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX RT1020 Reference Manual - SRK_REVOKE missing from fusemap?

780 Views
rshipman
Contributor V

FYI:

Regarding: i.MX RT1020 Processor Reference Manual, Rev. 1, 12/2018

On page 1190 (and other places such as page 1129) the manual refers to SRK_REVOKE fuse at 0x6F0h

However on page 1122 (Table 21-9. Fusemap Descriptions), location 0x6F0 is shown as reserved.

Thanks.

Labels (1)
0 Kudos
Reply
1 Reply

706 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello, 

The OCOTP base address is 401F_4000h. On page 1190, the 6F0h that you are seeing is the offset of the register HW_OCOTP_SRK_REVOKE in comparison to the OCOTP base address. So, the 6F0h that you are seeing on page 1190 is not related to the one in Table 21-9. 


Have a great day,
Victor

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply